技術支援

E5081A ENA-X 向量網路分析儀

  • 資源
  • 驅動程式、韌體和軟體
  • 培訓與活動
  • 智庫

資源

顯示 1 至 25 / 33
排序依據 :
日期
日期 標題
Filter Results
重新填寫
依內容類型
展示
Watch this demo to learn how the E5081A ENA-X network analyzer characterizes power amplifier behavior up to 44 GHz.
2023-07-17
新聞室
Midrange solution offers simplified test setup that accelerates characterization of power amplifier designs for 5G transmitters by up to 50%
2023-05-25
簡易說明書
Vector Network Analyzer Hardware and Software Promotions. Available for a limited time, take advantage of bundled promotions for Keysight’s new E5081A vector network analyzer (VNA) and software applications listed below.
2025-01-03
簡易說明書
Save 30% on a 4-port ENA-X with noise figure. Choosing the right options for your vector network analyzer based on your application just got easier, and less expensive. Selecting the necessary performance hardware and adding application-specific software gives you faster, more diverse insights at a...
2024-09-18
展示
Learn how to make power amplifier measurements with high accuracy.
2024-01-04
其他
Downloadable STEP of the E5081A mechanical drawing.
2023-08-18
使用者手冊
This manual provide guide to install the solid state drive kit.
2023-08-17
參考指南
Describes how to use ENA security features to protect and remove classified proprietary information stored or displayed in the instrument.
2023-06-13
快速入門指南
This poster provides a way to start using the E5081A ENA-X Vector Network Analyzer quickly.
2023-02-22
快速入門指南
The startup guide helps you to quickly install the instrument and provides you the requirements and information regarding the instrument.
2023-01-01
應用說明
Learn three practical RF calibration techniques to achieve accurate and repeatable RF test measurements, including vector calibration and scalar calibration.
2017-11-30
課程
A vector network analyzer (VNA) is a device used to measure the electrical properties of RF and microwave devices and networks. It does this by sending a signal down a transmission line and measuring the reflected and transmitted signals. The VNA then uses these measurements to calculate the...
Webinars
An interview with Dr. Joel Dunsmore, a world-renowned scientist and author on the topic of vector network analyzers (VNAs). In the video, Dr. Dunsmore discusses the theory of VNAs, as well as practical tips for using them. He covers a wide range of topics, including the different types of VNAs, how...
白皮書
Receivers only operate as well as their internal low-noise amplifiers perform. However, amplifiers prove to be the most challenging system component to characterize fully. Learn how the Keysight E5081A ENA-X network analyzer simplifies low-noise amplifier performance verification by using flexible...
2023-10-05
白皮書
This white paper examines the importance of power amplifier nonlinear characterization, time-domain versus frequency-domain characterization measurements, and the benefits offered by ENA-X network analyzer for high-power amplifier testing.
2023-05-24
說明檔
Download and install the simulator from https://www.keysight.com/find/e5080b-firmware. The CHM file is located under C:\Program Files\Keysight\Network Analyzer\Help\ENAENA. The help file does not show if it is saved in remote directory. You can copy it on different place in the local HDD. If you...
2023-09-29
簡易說明書
When your budget is limited or non-existent, but you want to have the equipment long term, get a great rate on Keysight’s latest RF and microwave test instruments. Our Elite Rental Partners offer budget friendly ways to Rent-to-Own Keysight test equipment with 50%+ of the payment credited toward...
2024-03-01
白皮書
This white paper examines the importance of power amplifier nonlinear characterization, time-domain versus frequency-domain characterization measurements, and the benefits offered by ENA-X network analyzer for high-power amplifier testing.
2023-06-27
簡易說明書
Available for a limited time, take advantage of bundled promotions for vector network analyzer’s (VNA) and enhanced time-domain analysis with TDR software application.
2024-10-31
應用說明
Noise figure is one of the key parameters that is characterized on the receiver component of these sub-systems. This application note compares the noise figure measurement capability of the ENA-X and PNA-X.
2024-09-01
應用說明
Noise figure is one of the key parameters that is characterized on the receiver component of these sub-systems. This application note compares the noise figure measurement capability of the ENA-X and PNA-X.
2023-10-23
展示
Watch this demo to learn how the E5081A ENA-X network analyzer characterizes T/R module behavior up to 44 GHz.
2023-08-23
展示
Watch this demo to learn how the E5081A ENA-X network analyzer characterizes low noise amplifier behavior up to 44 GHz.
2023-08-23
解決方案簡介
Method of Implementation (MOI) for DP cable Compliance Test Solution using Keysight Vector Network Analyzer, L8990M Switch Matrix and S94USBCB Compliance Test Software
2024-09-12
展示
Watch this demo to learn how the E5081A ENA-X network analyzer characterizes mixer behavior up to 44 GHz.
2023-08-23
顯示 1 至 25 / 33

驅動程式、韌體和軟體

培訓與活動

智庫

Mexico