何をお探しですか?
Keysight Introduces Software-Defined Handheld Analyzer
- New FieldFox C-model offers more than 20 vector network analyzer and spectrum analyzer options for upgrade and download, which are software licensing key enabled
- Enables engineers to pay only for the capabilities they need on a single, rugged handheld analyzer
- Provides accurate, comprehensive spectrum and network analysis down to 3 kHz
SANTA ROSA, Calif. July 20, 2023
Keysight Technologies, Inc. (NYSE: KEYS) is expanding its FieldFox portfolio with the new N9912C FieldFox Handheld Analyzer, a software-defined radio frequency (RF) testing platform offering field engineers more than 20 vector network analyzer (VNA), cable and antenna tester (CAT), and spectrum analyzer (SA) options for upgrade and download.
Field engineers conduct routine maintenance on and troubleshoot RF, microwave, and millimeter wave (mmWave) systems. During their work, they need to accurately measure a variety of devices or signals, including cables, antennas, and over-the-air (OTA) signals, to ensure robust signal quality and uninterrupted service. To make all of these crucial measurements in the field, engineers need multiple expensive network and spectrum analyzers as well as flexible equipment that can meet rapidly emerging test and measurement challenges.
The Keysight N9912C FieldFox Handheld Analyzer addresses this challenge by enabling engineers to mix-and-match software applications for their specific analysis needs on a single, handheld device. As a truly software-defined instrument, the FieldFox N9912C is fully upgradable with license-key activated maximum frequencies, analyzer types, bandwidths, and software applications.
The new FieldFox C-model, covering up to 10 GHz, offers the following benefits:
- Mix and match options – Offers unparalleled flexibility to create the right mix of VNA, CAT, and SA tools for any project's requirements with more than 20 downloadable software applications and license key activated frequency and bandwidth options. In addition, the maximum frequency coverages for any analyzer type are extendable for any existing N9912C by ordering an upgrade option.
- Pay only for what you need – Optimizes field instrument investment by enabling engineers to choose only the capabilities they need for their work in the field.
- Save time in the field with a single handheld – Eliminates the need to switch instruments with a single, rugged handheld analyzer that can be customized on the fly as testing needs evolve.
- High-performance analysis – Provides accurate, comprehensive spectrum and network analysis down to 3 kHz and up to 10 GHz, to test and troubleshoot a wide range of high frequency and wireless applications.
Vince Nguyen, Vice President and General Manager, Aerospace, Defense, and Government Solution Group at Keysight, said: "When engineers are in the field, they need flexible test solutions that can address challenges on the fly. With the truly software-defined FieldFox-C, engineers can quickly respond to new needs with a single, handheld analyzer that can be easily configured through software license keys covering frequency ranges, multiple analyzer types, and other software applications. With low entry pricing points that protect initial investments, the FieldFox-C is the all-in-one solution for multipurpose field testing."
Resources
About Keysight Technologies
At Keysight (NYSE: KEYS), we inspire and empower innovators to bring world-changing technologies to life. As an S&P 500 company, we're delivering market-leading design, emulation, and test solutions to help engineers develop and deploy faster, with less risk, throughout the entire product lifecycle. We're a global innovation partner enabling customers in communications, industrial automation, aerospace and defense, automotive, semiconductor, and general electronics markets to accelerate innovation to connect and secure the world. Learn more at Keysight Newsroom and www.keysight.com.
Keysight Contact:
Paul Erwin, Americas/Europe
+1 248 430–9075
[email protected]
Fusako Dohi, Asia
+81 42 660–2162
[email protected]
The new Keysight N9912C FieldFox Handheld Analyzer is a software-defined radio frequency testing platform offering field engineers more than 20 vector network analyzer, cable and antenna tester, and spectrum analyzer options for upgrade and download.
Need to contact Media Relations at Keysight?