何をお探しですか?
Keysight Delivers First 256 Giga-Samples Per Second Arbitrary Waveform Generator with Analog Bandwidth Exceeding 80 GHz
Enables R&D engineers to develop designs well beyond 160 GBaud
SANTA ROSA, Calif., September 20, 2022
Keysight Technologies, Inc. (NYSE: KEYS), a leading technology company that delivers advanced design and validation solutions to help accelerate innovation to connect and secure the world, announced the new M8199B arbitrary waveform generator (AWG), which provides R&D engineers a high-performance signal source for arbitrary signals that enables development of designs employing multi-level modulation formats (e.g. 64QAM) at well beyond 160 GBaud.
Applications beyond 128 GBaud demand a new class of generators that provide high speed, precision and flexibility at the same time. Keysight addressed these challenges with the company's new M8199B AWG which offers a high performing signal source for arbitrary signals with sampling rate up to 256 GSa/s and analog bandwidth exceeding 80 GHz, including up to eight synchronized channels operating simultaneously.
Keysight's new M8199B AWG provides research engineers the speed, bandwidth, precision, and flexibility to meet the challenges of next-generation applications, enabling data transmission greater than 400 Gb/s per lane in intensity-modulation/direct-detect (IM/DD) and greater than 1.6 Tb/s per carrier in coherent optical communications.
"Today's applications and services generate vast amounts of artificial intelligence workloads in the data center. New electrical and optical designs are required to handle these workloads within reasonable bounds of energy consumption," said Dr. Joachim Peerlings, vice president and general manager of Keysight's Network and Data Center business. "We are pleased with Keysight's continuous efforts to deliver first-to-market solutions that support our customers to connect and sustain our planet and take the next step in the race for higher data transmission rates."
Built with Keysight-custom technology, the M8199B AWG offers the following key benefits:
- Intensity-Modulation/Direct-Detect (IM/DD) and coherent optical applications: provides the flexibility needed for advanced research on new modulation formats to boost transmission rates to the next level. The M8199B AWG matches with high-speed research experimenting using multi-level pulse-amplitude modulation (PAM), quadrature-amplitude modulation (QAM) formats and other proprietary modulation formats at symbol rates approaching 200 GBaud. In addition, it provides stress signals to test next generation electro/optical components, digital signal processor application-specific integrated circuits (DSP-ASICs), and new algorithm concepts for multi-terabit transmissions systems.
- Wideband radio frequency (RF) signal generation in wireless and aerospace/defense applications: addresses the latest developments in radar and wireless technologies which require generation of high-quality signals with modulation bandwidths well beyond 10 GHz. Generating those signals on an intermediate frequency (IF) rather than on quadrature signals is another important capability to support these applications.
- Physics, chemistry, and general-purpose electronics research: enables users to generate any arbitrary waveform that can be mathematically described, including ultra-short pulses, wideband RF pulses, and chirps needed to investigate in applications such as chemical reactions, elementary particle excitation and quantum effects.
Availability
Keysight's M8199B AWG will be available in October 2022.
Additional information about Keysight's new M8199B arbitrary waveform generator (AWG) is available at
https://www.keysight.com/us/en/products/arbitrary-waveform-generators/m8100-series-arbitrary-waveform-generators/m8199b-256-gsa-s-arbitrary-waveform-generator.html.
About Keysight Technologies
Keysight delivers advanced design and validation solutions that help accelerate innovation to connect and secure the world. Keysight's dedication to speed and precision extends to software-driven insights and analytics that bring tomorrow's technology products to market faster across the development lifecycle, in design simulation, prototype validation, automated software testing, manufacturing analysis, and network performance optimization and visibility in enterprise, service provider and cloud environments. Our customers span the worldwide communications and industrial ecosystems, aerospace and defense, automotive, energy, semiconductor and general electronics markets. Keysight generated revenues of $4.9B in fiscal year 2021. For more information about Keysight Technologies (NYSE: KEYS), visit us at www.keysight.com.
# # #
Additional information about Keysight Technologies is available in the newsroom at https://www.keysight.com/go/news and on Facebook, LinkedIn, Twitter, and YouTube.
Keysight Contact:
Geri Lynne LaCombe, Americas/Europe
+1 303 662–4748
[email protected]
Fusako Dohi, Asia
+81 42 660–2162
[email protected]
Need to contact Media Relations at Keysight?