Loading...

Showing 20 of 760

Sort:
Popularity
Popularity Newest Relevancy
Popularity Newest Relevancy
The Essential Signal Generator Guide Building a solid foundation in RF — Part 2

Added to favorites

Removed from favorites

The Essential Signal Generator Guide Building a solid foundation in RF — Part 2

Navigating the numerous specifications and features of signal generators can be challenging. This white paper series helps by explaining various modulation schemes, the importance of spectral purity, and the impact of distortion. Additionally, it explores how application software can enhance productivity. Signal generators are essential for meeting customer requirements for robust and reliable high-speed wireless connections, which are crucial for business success. To address market demands, selecting the right signal generator is vital. Complex modulation schemes, necessary for increasing spectral efficiency and achieving higher data rates, rely on accurate and stable signal generators. Signal generators can be either digital (vector) or analog. Vector signal generators produce complex, digitally modulated signals, while analog signal generators produce continuous wave signals with basic modulation. The choice depends on the specific application and testing requirements. Generating an RF signal requires a metrology-grade signal generator with excellent distortion and spurious characteristics to ensure high spectral purity. The frequency accuracy of a signal generator depends on the stability of the reference oscillator and the time since the last calibration. Overall, signal generators are indispensable for evaluating applications that rely on radio frequencies, such as GNSS, 5G, avionics, and radar, ensuring reliable and efficient performance.

The Ins and Outs of Satellite Communications

Added to favorites

Removed from favorites

The Ins and Outs of Satellite Communications

Getting a refresh on the fundamental aspects impacting satellite communications (SATCOM) is more critical than ever, as new market opportunities fuel the commercialization of space. Much of this activity focuses on the low Earth orbit (LEO) because of decreasing launch costs and the increased functionality of smaller, lighter satellites. These satellites support various use cases, including fifth-generation (5G) and eventually sixth-generation (6G) cellular non-terrestrial networks (NTN). Examples include communications coverage over vast distances and enhanced situational awareness on the ground for military and critical communications. Rapid development creates unique challenges when designing and building these complex systems, including the orbits involved, link budgets, antennas, modulation standards, and the need to thoroughly test these systems. By understanding the various factors and their impact on design, satellite developers can optimize performance throughout the satellite development life cycle, regardless of orbit and application. To ensure optimized performance throughout the satellite life cycle, manufacturers and network operators must account for unique variables such as Doppler shift, ionosphere distortion, and atmospheric losses. They also need to ensure that satellite systems can navigate the crowded electromagnetic spectrum — a landscape that will only grow more congested as commercialization continues. Testing for situational awareness will be a significant part of effectively managing space traffic as new systems go into orbit. By modernizing your strategies to account for these and other challenges, you can play a pioneering role in the next phase of the space gold rush.

Viewed 20 of 760 Load More