技術支援

N7019A USB Type-C® Active Link 測試夾具

  • 資源
  • 驅動程式、韌體和軟體
  • 培訓與活動
  • 智庫

資源

顯示 1 至 9 / 9
排序依據 :
日期
日期 標題
Filter Results
重新填寫
依內容類型
新聞室
Keysight’s new test and measurement solutions accelerate development, implementation, and deployment of new USB 80Gbps devices
2022-10-19
新聞室
Keysight solutions enable customers to develop and validate USB interfaces for new USB 80Gbps implementations quickly and accurately
2022-11-08
產品規格書
Use the N7019A to access all your Type-C signals in a live link. The acquired signals can be used for debug or decoded with USB-PD, USB 2.0, USB 3.2, or USB4 Protocol Decode Software.
2020-03-03
型錄
This document provides an overview of Keysight High-Speed Computing Solutions, including PCI Express, DDR test, and USB transmitter and receiver test.
2024-04-10
使用者手冊
This guide describes how to set up, configure, and use the N7015A, N7016A, N7017A, N7018A, and N7019A Type-C test fixtures to perform integrated testing for various interfaces supported over Type-C.
2022-12-14
影片
During this on-demand webinar, we will cover the latest updates in the USB Type-C™ ecosystem, including USB, DisplayPort (DP), and Thunderbolt. USB Type-C™ and USB-C™ are trademarks of the USB Implementers Forum.
2022-04-07
應用說明
This application note provides an overview of Type-C link debug and optimization using USB4 as an example. Learn how a Lane Adapter State Machine describes the behavior of the logical link layer and get step-by-step procedures for debugging and optimizing the USB link.
2022-02-14
影片
Learn more about the differences between testing Thunderbolt 3 and USB4 using the Infiniium UXR-Series oscilloscope, and discover techniques to avoid USB4 testing pitfalls. At the end of the webinar, we will share some upcoming changes to the CTS and test method.
2021-07-13
應用說明
This document explores testing USB Type-C power delivery, addressing challenges and recommending test solutions.
2023-09-15
顯示 1 至 9 / 9

驅動程式、韌體和軟體

培訓與活動

智庫

繁體中文