尋找感興趣的產品?
Keysight’s New Parallel Parametric Test System Delivers High Throughput and Cost-Effective Wafer Test
New probe card adapter and SPECS software supports smooth production ramp-up
SANTA ROSA, Calif. November 30, 2021
November 30, 2021 – Keysight Technologies, Inc. (NYSE: KEYS), a leading technology company that delivers advanced design and validation solutions to help accelerate innovation to connect and secure the world, announced the new Keysight P9002A parallel parametric test system, which provides high throughput and cost effective wafer test to accelerate time-to-market in R&D and lower cost-of-test in manufacturing.
The global semiconductor shortage has created a growing demand for semiconductors in the automotive industry, as well as digital devices and home appliances. Ongoing technology innovation in semiconductors is progressing rapidly, and the industry is facing a variety of technical challenges to adapt new materials, as well as miniaturization and 3D packaging processes. In addition, the complicated device design to target commercial applications like 5G, data center, artificial intelligence (AI) and automotive are increasing test parameters.
To address this challenge and enable manufacturers to quickly ramp capacity, Keysight has delivered the new P9002A parallel parametric test system, which offers cost-effective wafer test with high throughput, as well as a flexible option structure for up to 100 channels parallel test resources, including test capabilities required for parametric tests at each test resource. Keysight's P9000 series provides software compatibility with SPECS software on 4080 series parametric testers, enables customers to utilize their existing test programs and test plans with data correlations.
Keysight's new P9002A parallel parametric test system delivers the following key customer benefits:
- Ability to add options based on test requirements, with license structure for cost effective budgeting.
- Unique parametric test technologies and fast capacitance measurement generates improved throughput over the 4080 series parametric testers.
- System compatibility and data correlation with Keysight 4080 series parametric tester, enables customers to utilize their existing tester programs, test plans and probe cards with 4080-compatible probe card adapter to minimize the cost of building with a new P9002A test environment.
"Keysight is delighted to support the development and manufacture of ever-evolving semiconductors with advanced measurement solutions, such as the P9002A test system," said Shinji Terasawa, vice president and general manager of Keysight's Wafer Test Solutions. "This new solution reflects Keysight's commitment to helping solve our customers business challenges with proven experience and expertise in parametric testing."
About Keysight Technologies
Keysight delivers advanced design and validation solutions that help accelerate innovation to connect and secure the world. Keysight's dedication to speed and precision extends to software-driven insights and analytics that bring tomorrow's technology products to market faster across the development lifecycle, in design simulation, prototype validation, automated software testing, manufacturing analysis, and network performance optimization and visibility in enterprise, service provider and cloud environments. Our customers span the worldwide communications and industrial ecosystems, aerospace and defense, automotive, energy, semiconductor and general electronics markets. Keysight generated revenues of $4.9B in fiscal year 2021. For more information about Keysight Technologies (NYSE: KEYS), visit us at www.keysight.com.
# # #
Additional information about Keysight Technologies is available in the newsroom at https://www.keysight.com/go/news and on Facebook, LinkedIn, Twitter, and YouTube.
Keysight Contact:
Geri Lynne LaCombe, Americas/Europe
+1 303 662–4748
[email protected]
Fusako Dohi, Asia
+81 42 660–2162
[email protected]
Need to contact Media Relations at Keysight?