Used Equipment Store

Account Benefits

Get a customised view of the Used Equipment Store

Manage your details to get quick responses by the team

Stay up-to-date on specials, prices and availability

已经有账户? 登录

Create Your Account

Sign up to receive marketing or promotional emails from Keysight

By submitting this form, you are providing Keysight with your personal data. For information on how we use this data, see the Keysight Privacy Statement.

How to Test a Resistor with a Multimeter: A Step-by-Step Guide

Your browser limits use of the Used Keysight Equipment website.
Please consider switching to a current version of Chrome, Firefox, Edge or IE11 to use this site.

此页面暂时不提供中文版本。我们计划在不久的将来提供更多内容并支持中文。

Ever been stumped by a seemingly simple electronic gadget acting up? Maybe it's your beloved guitar pedal giving you tone trouble, or that DIY project refusing to function. It can be maddening!
In such situations, the humble resistor is often the reason. This tiny component can wreak havoc if not working correctly. But how do you figure out whether it is doing its job?
Enter the multimeter, an engineer's best friend! This tool helps diagnose issues in electronic circuits and components like resistors.
Imagine being able to identify faulty resistors quickly, fix them promptly and bring your projects back to life swiftly! Wouldn't it be great to have such an easy solution? Let's begin a step-by-step guide on how to effectively use a multimeter.

Find Multimeters on Sale Now!

最多可以选择3台仪器进行对比

取消
还可以挑选另一台仪器进行对比
还可以挑选另一台仪器进行对比
还可以挑选另一台仪器进行对比

Understanding Resistors and Their Role in Electronics

Resistors are pivotal components in electronic circuits. They control the flow of current, essentially acting as traffic cops on a busy road.
You can imagine resistors as narrow passages or bottlenecks where electrical currents have to squeeze through. The more resistance a resistor has, the narrower this passage is, allowing less current to pass through.

ENA Vector Network Analyzers

Perfect Signals, Perfect Performance

See E5080B Special Offers

Common Types of Resistors

Type of ResistorDescriptionKey Characteristic
Fixed ValueOffers a constant level of resistanceResistance remains the same regardless of temperature or light exposure
VariableAllows for adjustment of resistance as neededResistance value can be manually varied
ThermistorReacts to changes in temperatureResistance increases or decreases with temperature changes
Light Dependent (LDR)Sensitive to the amount of lightResistance changes based on light exposure

The Importance of Resistors in Electronic Circuits

Resistors play a crucial role in shaping electronic circuits' behavior. They're like puzzle pieces that fit together to form an operational circuit.
Without resistors, current would flow uncontrolled through the circuit, possibly causing damage or unpredictable operation. Adding resistors into a circuit allows you to regulate and control this current flow precisely, allowing for more predictable performance.
For instance, imagine a simple LED lighting setup without any resistor involved. The high level of current could burn out the LED quickly, but with proper resistance added to limit the current flow, the LED can function safely and efficiently.

Getting Familiar with Multimeters

A multimeter, also known as a VOM (Volt-Ohm meter), is an essential tool for any electrical engineer. It's versatile and reliable, like the Swiss Army knife of electronic testing.

Types of Multimeters

Analog and digital multimeters are the two primary varieties, with analog models featuring a needle for readings and DMMs providing measurements on an LCD display.

FeatureAnalog MultimeterDigital Multimeter
Best Suited ForWatching trends or quickly checking circuitsSituations where precision is crucial
AccuracyLess accurate compared to digitalMore accurate, ideal for precise measurements
Ease of ReadingRequires interpretation of the needle positionEasier to read with a direct digital display
Ideal UseGood for general, non-precise measurementsPerfect for detailed, accurate readings

Key Functions of a Multimeter

Multimeters are used to measure many things in electronics, including voltage, current and resistance. The versatility of these instruments makes them invaluable for troubleshooting electrical problems in everything from industrial equipment to small household appliances. 

Safety Precautions While Using a Multimeter

A multimeter can pose certain risks if not used correctly. So let's explore some crucial safety precautions to ensure your safety while using a multimeter. 

    Avoid High Voltage Measurements Unless Necessary

    When dealing with a multimeter, abstain from measuring high voltage unless absolutely necessary. 

    • High voltages can cause severe injuries or even death if handled improperly. 
    • Always double-check the range setting on your multimeter before connecting it to any circuit.

    Use Correct Probes And Leads

    Properly rated probes and leads are key in ensuring safety during resistor testing with a multimeter. Make sure you're using probes that meet or exceed the maximum voltage of what you're measuring – this will help prevent electrical shocks or shorts that could damage equipment or lead to injury.

    Regular Inspection Of Your Multimeter Is Essential

    Inspect your multimeter regularly for any signs of damage, such as cracked casing, frayed wires, or damaged probes. Any sign of physical damage should be addressed immediately by replacing parts as needed.

    Always Disconnect The Test Leads Before Replacing The Battery Or Fuses

    Popping open the back cover while the test leads are connected might expose live circuits which poses a significant risk of electrical shock. So always disconnect the test leads before you open up your multimeter.

    Take Precautions When Working With Capacitors

    Capacitors can hold charge long after power has been removed from a circuit, so be sure to discharge capacitors before testing resistance or continuity with your multimeter. This will protect both you and the device from any unexpected shocks.
    These precautions are not exhaustive but serve as fundamental safety practices when using a multimeter for resistor testing or other electronic component tests. Remember that safety should never be compromised – always follow manufacturer guidelines and use proper protective equipment when handling electronic devices.

    Key Takeaway
    While a multimeter is crucial for testing resistors, it's key to prioritize safety. Avoid high voltage measurements unless needed, and use the right probes and leads. Regularly inspect your device for wear or damage, disconnect test leads before replacing batteries or fuses, and be careful when working with capacitors. Always remember: safety first.

    Setting Up Your Multimeter for Resistor Testing

    Before you start testing a resistor, it's crucial to set up your multimeter correctly. No matter what type of multimeter you have, we'll help guide you through the setup process. 

    Choosing the Right Mode

    The first step is to choose the right mode on your multimeter. For testing resistors, we need to use Ohm (Ω) mode since resistance is measured in ohms.

    Selecting Appropriate Range

    Understanding range selection is key when using a manual-ranging meter as opposed to an auto-ranging one.

    • Select a resistor range that covers the expected reading in its middle 60%, avoiding both the high and low ends of the scale. 
    • If you’re unsure about anticipated values, start with higher ranges then gradually come down until you get accurate readings.

    Preparing Your Probes

    The probes are just as important in obtaining reliable measurements as proper setup itself.
    To get started:

    • Carefully plug the black probe into the common terminal often marked 'COM'. It may also be color-coded with black.
    • The red probe goes into VΩmA port – commonly indicated by voltage (V), resistance (Ω), and current (mA) symbols. This is where voltage, resistance, and low-current measurements are made.

    You're now set to start resistor testing.

    Check the Battery

    Before beginning any tests with your multimeter, ensure the battery is fully charged or replace it if necessary, as a low battery can lead to inaccurate readings. 

    Check the battery connections for proper fit and look for any signs of corrosion. It's also a good practice to perform a quick preliminary test to confirm the multimeter's accuracy.

    Step-by-Step Guide to Testing a Resistor with a Multimeter

    Testing resistors is crucial for maintaining electronic circuits. Here's how you can go about assessing a resistor with the help of a multimeter.

    1. Prepare Your Workspace

    Start by ensuring your workspace is clean and well-lit, reducing the risk of errors or accidents during testing.

    2. Set Up the Multimeter

    First, ensure the multimeter is powered down prior to configuring. Turn the dial on your digital multimeter to measure resistance (Ω).

    3. Connect Probes to Resistor

    Connect one probe (either red or black) to each end of the resistor – color does not matter when measuring resistance as current flow isn't involved here.

    4. Testing The Resistance Value Of A Resistor

    Make sure not to touch both probes together while taking measurements because this may cause an inaccurate reading.
    To check if there are any variations in resistance values, switch between different ranges on your multimeter. By doing so, you'll get more accurate readings even from smaller resistors. Once done, compare these readings with manufacturer data sheets to confirm accuracy. If discrepancies occur consistently, it might be time for professional calibration.

    5. Switch Off and Disconnect

    When finished with your measurements, always remember to turn off the multimeter and disconnect all connections.

    6. Notes on Measurements

    Check out our comprehensive guide: How to Measure Current with a Multimeter: A Guide for Engineers. This guide offers detailed insights and tips that can significantly enhance your understanding, improving the efficiency and reliability of your circuits.

    Oscilloscopes

    Solve Signal Issues Before They Escalate

    See MXR608A Special Offers

    Common Mistakes to Avoid When Testing Resistors

    Despite the simplicity of testing resistors, errors can sneak in if you're not careful. Let's explore some common errors and strategies for avoiding them.

    Mistake 1: Incorrect Multimeter Setting

    The first mistake is using incorrect settings on your multimeter. This could lead to inaccurate readings or even damage your resistor. It's crucial to set your multimeter to the resistance mode (often symbolized by an "Ω"). Also, remember that selecting a range too low for the resistor being tested may overload and possibly damage the meter.

    Mistake 2: Not Accounting for Tolerance

    Every resistor has a tolerance rating, which tells you how much its actual resistance might vary from its nominal value. Forgetting about this can make you think your resistor is faulty when it isn't. Make sure you understand resistor tolerances before drawing conclusions based on measurements.

    Mistake 3: Ignoring Lead Resistance

    The leads of a multimeter have their own resistance which can affect measurements especially when dealing with very high or low-value resistors. To fix this issue, use the 'relative' function present in most digital multimeters or manually subtract lead resistance from measured values.

    Mistake 4: Holding Resistor Leads During Measurement

    This mistake stems from an overlooked fact – our bodies conduct electricity. While measuring small resistances, the resistance of your body can significantly impact readings if you're holding the leads. Always handle only the insulated part of the probe while testing resistors.

    Mistake 5: Not Checking for Resistor Damage

    Physical damage to a resistor can affect its performance but is often overlooked during troubleshooting. Always inspect resistors for any visible signs of damage like charring, discoloration, or cracks before conducting tests with a multimeter.

    Key Takeaway
    Be wary of common resistor testing pitfalls: don't misuse your multimeter settings, overlook the importance of tolerance, or ignore lead resistance. Avoid holding the resistor leads during measurement and always inspect for physical damage before testing. Lastly, remember to disconnect resistors from circuits prior to assessing them with a multimeter.

    Troubleshooting Problems During Resistor Testing

    It is not uncommon to encounter issues when resistor testing with a multimeter. Here are some tips to help you manage the difficulties encountered during resistor testing with a multimeter.

    Inaccurate Readings

    The first hurdle could be getting inaccurate readings. This usually happens when the test leads aren't properly connected or if there's a problem with the resistor itself. Make sure that your connections are secure and clean – dust can sometimes interfere with results.
    If you're still seeing inconsistent numbers, try swapping out the resistor for another one. It might just be that your original component has worn out over time.

    Multimeter Not Responding

    Another issue could be your multimeter not responding at all while attempting to measure resistance. If this happens, check whether it's in the correct mode (Ohm) and range appropriate for the resistor being tested.

    Error Messages Displayed On The Screen Of The Multimeter

    At times, your multimeter may start showing error messages. One common message is 'OL', which means Overload. When you see this, it typically suggests either the resistance under test exceeds the maximum range of the meter or the leads aren't connected correctly.
    If adjusting connections doesn't fix it, consider changing the multimeter's range or testing another resistor to confirm if the issue lies with the original component.

    Zero Reading on Multimeter

    Getting a zero reading when you know there should be some resistance? That could mean your resistor is shorted. This happens when the path inside the resistor that creates resistance gets bypassed, causing electricity to flow freely without any restriction.
    To resolve this, try using a different resistor that you know is good and compare readings. If they match up well, then likely your initial part was faulty.

    Key Takeaway
    Running into issues while testing a resistor with a multimeter is common. These could include inaccurate readings, unresponsive multimeters, error messages or zero readings on the meter. Each problem has its solution: check your connections and clean them if necessary; make sure you're using the correct settings on your meter; swap out potentially faulty resistors with one that you know is good.

    Importance of Accurate Resistor Testing in Engineering Applications

    Accuracy in resistor testing is a cornerstone for any engineering application. It's not only about obtaining accurate figures; it's also about guaranteeing that systems operate as they should.
    When we test resistors, we're looking to measure resistance accurately. Inaccurate measurements can lead to circuit malfunction or even failure, which could have severe consequences in applications such as aviation electronics and medical devices.

    Signal Analyzers

    Rugged Precision, Anytime

    See N9020 Special Offers

    Ensuring System Functionality

    A slight variation from the desired resistance value might seem insignificant at first glance. For example, imagine driving your car with faulty brakes due to inaccurate resistor values within its electronic control unit (ECU). The potential danger is clear—accuracy matters because lives depend on it.

    Reducing Costs

    Not only does accurate resistor testing ensure safety—it also saves money. Faulty components due to inaccurate readings can lead to costly repairs or replacements. 

    For instance, if a source measure unit incorrectly reads a critical power supply component’s resistance during production line tests, that part may fail prematurely once deployed causing downtime and additional expenses for replacement parts and labor.

    Ensuring Compliance

    Another aspect to consider is regulatory compliance. Many engineering applications must meet specific industry standards, and accurate resistor testing helps achieve this.
    In the medical field, devices such as heart monitors demand precise resistance values for accurate functioning. Any deviation from these could signify non-compliance with FDA regulations. This might lead to serious consequences like product recalls or even legal issues.

    Advanced Techniques for Resistor Testing

    There are more advanced techniques that can give you a deeper understanding of the performance and reliability of your resistors. These methods often require a higher level of skill but provide invaluable insights for complex circuits or troubleshooting.

    Using Resistance Decade Boxes

    One technique involves using resistance decade boxes. These devices let you dial in precise resistance values, which is handy when working with sensitive electronics or calibrating equipment.
    You connect the box across the resistor under test and adjust its value until the multimeter reads zero volts (indicating no current flow). This method helps identify deviations from nominal resistance values, vital in high-precision applications.

    Employing Kelvin Connection Technique

    The Kelvin connection technique, also known as 4-wire measurement, offers another advanced approach. It eliminates lead wire resistance errors by using two pairs of leads. 

    One pair supplies constant current while the other measures voltage drop directly over resistor terminals. This provides highly accurate readings even on low-value resistors where lead wire resistance could otherwise skew results significantly.

    Understanding Temperature Coefficient Impact

    Understanding the temperature coefficient of resistance is another key to advanced resistor testing. All resistors exhibit some change in resistance value with temperature variation, but this can become significant in certain applications like power electronics or harsh environments.
    By heating a resistor and measuring its resistance at various temperatures (using precise thermal control equipment), you can characterize its temperature coefficient accurately. This data is vital for predicting circuit performance under varying conditions.

    FAQs About How to Test a Resistor With a Multimeter

    How do you check a resistor with a multimeter?

    Set your multimeter to the resistance setting. Connect one probe to each end of the resistor. For analog multimeters, ensure to zero the device before measuring for accurate results. Read the measurement displayed.

    How do you know if a resistor is bad?

    A resistor might be faulty if the multimeter shows an open circuit or infinite resistance. Additionally, check for visual damage like burns or cracks on the resistor.

    How to measure resistance with a multimeter?

    Select the 'ohms' mode on your meter. Touch the probes to both ends of the resistor. The reading should match the specified resistance within the tolerance range. Remember, temperature can affect resistance readings.

    How do you test the effectiveness of a resistor with a multimeter?

    Gauge its effectiveness by comparing the measured value against the manufacturer's specifications. Ensure the resistor is disconnected from any circuit for accurate measurement. A significant deviation may indicate performance issues.

    What should be done for accurate readings in analog multimeters?

    For analog multimeters, it's important to zero the device and check that the meter itself isn't adding resistance to the measurement.

    What is the impact of temperature on resistance measurements?

    Temperature can alter resistance values. High temperatures typically increase resistance, so consider the environment when measuring.

    Is it necessary to remove the resistor from the circuit for testing?

    Yes, if possible. Testing a resistor while it's still in a circuit can lead to inaccurate readings due to the influence of other components.

    How does a multimeter’s battery condition affect measurements?

    For digital multimeters, ensure the battery is in good condition as a low battery can lead to inaccurate readings.

    Conclusion

    This guide has provided the skills needed to test resistors using a multimeter. We’ve discussed the critical role of resistors in electronic circuits and how to set up and use a multimeter safely and accurately. The step-by-step approach has equipped you to avoid common mistakes and troubleshoot problems effectively. 
    Remember, precise resistor measurements are key in engineering, and with these techniques, you're ready to confidently tackle complex circuit issues.

    Whenever You’re Ready, Here Are 5 Ways We Can Help You

    1. Browse our premium used network analyzers, oscilloscopes, signal analyzers and waveform generators.
    2. Call tech support US: +1 800 829-4444 
      Press #, then 2. Hours: 7 am – 5 pm MT, Mon– Fri
    3. Talk to our sales support team by clicking the icon (bottom right corner) on every offer page
    4. Create an account to get price alerts and access to exclusive waitlists.
    5. Talk to your account manager about your specific needs.

    Subscribe to Get Our Latest News, Updates, and Articles.

    Get Email Updates