The S95088B allows users to set calibrated, arbitrary phase differences between two signal sources on the M980xA PXI VNAs.

Highlights

  • Control the relative phase between the two internal sources and/or external signal generators
  • Provide calibrated, electronic loads to an amplifier under test
  • Sweep the phase of the load while maintaining the constant reflection-coefficient magnitude
  • Requires 2 or more M980xA PXI VNA modules configurations (available 2 or more sources in one measurement site.)

The S95088B allows users to set calibrated, arbitrary phase differences between two signal sources. The sources can be the analyzer’s internal sources or external signal generators routed through the analyzer’s test set. The phase difference can be fixed, or swept between two specified phase values. S95088B also controls the relative power level between the sources using the receiver-leveling feature.

The S95088B is targeted for active-load control, where the analyzer provides a precise, electronically settable impedance to the output port of a device, while gain and output power are measured. This capability can be combined with external load-pull software to create traditional load-pull power contours.

Extend the Capabilities of Your Product

Want help or have questions?

Worldwide