What is quantum information technology?

Quantum information technology (QIT) is a rapidly advancing field that leverages quantum mechanics to manipulate information in novel ways, leading to vast improvements over classical technologies. QIT exploits quantum phenomena like superposition and quantum entanglement to overcome the challenges of information storage, processing, transmission, and security. The field of QIT encompasses a spectrum of applications that leverage quantum systems, including quantum computing, quantum sensing, and quantum communications.

We are on the brink of an information technology (IT) revolution enabled by quantum mechanics. Achieving it will require collaborative research to address the challenges inherent in trying to control the properties of the quantum realm. Every breakthrough deepens the understanding of quantum properties and leads to new architectures and innovations that bring us closer to achieving quantum supremacy and commercially viable applications.

QIT essentials

Quantum: Discover the possibilities

Tap resources to help you understand quantum mechanics and the technologies it powers.

An icon representing quantum information technology

Quantum fundamentals
Understand basic quantum concepts and what is necessary to realize its full potential.

An icon representing quantum sensing technology

Quantum sensing
Learn about quantum sensing theory, applications, and enabling technologies in this course.

An icon of a quantum computer representing quantum information technology

How to build a superconducting quantum processor
Explore the core concepts and components needed to build a superconducting quantum processor.

The fundamentals of quantum mechanics

An icon of a puzzle with one piece out of place

Believing that the natural laws governing the universe are determinable, Einstein said of quantum mechanics, “God tirelessly plays dice under laws which he has himself prescribed.” The idea that the state of the universe at a point in time can determine its state at all other times is a core tenet of classical mechanics and, indeed, science.

Quantum research in the early 20th century revealed an aberrant realm where systems deviate from the strict rules of classical mechanics, electricity and magnetism, and general and special relativity.

What are the key distinctions between classical and quantum mechanics?

An illustration of a puzzle piece

The Heisenberg uncertainty principle (HUP) represents a shift from classical predictability to quantum probability and highlights the differences between classical and quantum mechanics. HUP asserts that the more precisely we know one property of a particle, the less precisely we can determine other properties.

For example, the more precisely you measure location, the greater the uncertainty you would have in the speed, and vice versa. This is because in order to see the particle, you must shine light on it; to measure its location, the light must possess short wavelengths. However, because these short-wavelength light sources are energy-dense, they disturb the particle’s speed. Therefore, the act of trying to accurately measure where a particle is makes it difficult to measure its speed with any precision.

HUP serves as a gateway to understanding the profound differences between classical and quantum mechanics, including superposition, qubits, and entanglement.

Key quantum mechanics concepts to understand

Core components of quantum information technology

Qubits

Quantum bits, or qubits, are the building blocks of QIT. They are the most fundamental units of quantum information. Classical data bits exist in two states, written as 0 and 1. While they can take many forms and perform a vast array of functions, a bit must always be in either a 0 state or a 1 state.

If you picture a sphere, the surface represents all of the possible states of a qubit. Classical bits are like points located only at the poles of the sphere, fixed in either the 0 or 1 state. Qubits can occupy any point along the sphere’s surface, representing an infinite number of possible states. This freedom allows qubits to encode and process exponentially more information than classical bits do.

Qubits do this through superposition and entanglement. Superposition supplies their remarkable flexibility and power. Entanglement enables qubits to become correlated in such a way that the state of one qubit instantly influences another, regardless of the distance between them. These unique properties shatter the constraints of classical bits and allow qubits to exist in a rich, complex state space. They can encode and process quantum information in ways that promise meaningful advancements in computation, communication, and cryptography.

Superposition

Going back to the sphere analogy, superposition lets qubits carry information between the 0 and 1 states at the same time. In classical physics, objects have definitive properties at any given time. In quantum physics, however, particles like electrons, photons, and atoms can exist in a combination of states simultaneously, known as superposition.

Schrödinger’s cat is a well-known thought experiment that describes how the quantum superposition of non-decayed and decayed radioactive nuclei can influence superposition on a macroscopic level. In this gruesome scenario, a scientist places a cat in a box with a radioactive mechanism that controls a vial of poison. The moment of the poison’s release is unknown; thus, the cat occupies a state of both life and death until we open the box and observe its fate.

Quantum mechanics cannot predict the fate of Schrodinger’s cat. Instead, it provides us with the probability of which state we will find the cat in when we open the box across a large set of identical experiments.

Superposition is what enables quantum bits (qubits) to perform highly complex functions by representing multiple states simultaneously. Going back to the sphere analogy, superposition states have amplitudes and enable qubits to carry information between the 0 and 1 states at the same time. As the number of qubits increases, the number of available probability amplitudes increases exponentially. It is this property that gives quantum technology the probability to dramatically accelerate the speed of computational tasks relative to their classical counterparts.

Quantum entanglement

Entanglement is the key to harnessing quantum information processing. Quantum entanglement occurs when the states of two or more particles become correlated such that the state of one particle instantaneously influences the state of another, irrespective of the distance between them.

This correlation persists when the entangled particles separate, even by long distances. Without entanglement, each qubit exists independently on the sphere, in its own world with its own possible states. When qubits become entangled, however, their positions become intricately linked, enabling them to explore a broader range of states than they could individually.

The coordinate movements of entangled qubits on the surface of the sphere maximize the flexibility enabled by superposition. If you perform a measurement on one entangled qubit and collapse it to a specific state, the state of the other qubit is determined instantaneously as well, regardless of where on the sphere it resides. Entanglement enables qubits to leverage their collective quantum nature to unlock the potential for highly efficient computation, secure communication, and novel cryptographic protocols.

A diagram of the Bell test for entangled qubits

This graph depicts the two observers, Alice and Bob, sharing an entangled state.

Quantum decoherence

While the previously explained properties enable qubits to hold much more computational power than classical bits, a big challenge for quantum computers is a phenomenon called quantum decoherence.

Quantum decoherence occurs when a system interacts with elements in the environment, such as air, thermal radiation, or a non-demolition measurement apparatus. To understand decoherence, you must first understand quantum coherence. In its simplest form, coherence refers to the measure of the relationship between different possible states within the quantum system. This information is necessary for the quantum computer to function. Isolation maintains coherence.

Quantum decoherence occurs when the system interacts with its internal and external environment. When this happens, the system’s information and the environmental information comingle, making it difficult to distinguish quantum system signals from environmental noise. Qubit states are unstable, and different environmental factors can affect the state of a qubit in an unknown way, similar to noise in scientific measurements. A stray photon or a fluctuation in temperature can cause an energy shift in the qubit. As a result, the state moves closer to collapse.

 

Quantum interference

In addition to the influence of environmental factors, qubits in an entangled system can affect the state of other qubits. Quantum interference occurs when the probability amplitudes of different states a qubit can take interfere with each other, causing either constructive or destructive interference effects. Each trajectory corresponds to a different sequence of operations applied to the qubit.

Constructive interference occurs when the probability amplitudes of trajectories align and reinforce each other, increasing the likelihood of finding a qubit in certain states. Destructive interference occurs when the trajectories’ probability amplitudes cancel each other out, reducing the probability of finding the qubit in certain states.

Quantum interference plays a crucial role in quantum information processing. By manipulating the quantum states of qubits and controlling the interference effects, quantum algorithms can exploit interference to enhance computational efficiency and solve problems considered intractable for classical systems.

Quantum error correction

In order to combat quantum decoherence and noise in the system, quantum computers use entanglement and interference to help correct errors. Classical error correction is easier to work with. A bit can be only 0 or 1, and an error can only be a bit flip. To combat this, classical computers encode their bits redundantly. Instead of using 1 bit to represent 0 or 1, they use multiple, such as 000 or 111. An error might look like 010, where we can assume that this means 0, and the middle bit just had an error. This also works because bit flips in classical bits are rare.

Qubits are different. While their state can deviate from expectations, we are unable to observe the shift because of the measurement collapse that would result from observations. The way we work with this is similar to classical bits in that we encode the qubits redundantly but put them in an entangled state with other ancillary qubits. In the entangled state, each qubit’s state connects to the other qubits’ states. This way, we can extract information from an ancillary qubit and infer the state shift in the computational qubit and thus correct it.

Quantum information processing and communication

An icon representing quantum information technology

The properties of quantum mechanics underpin the reasons QIT promises revolutionary potential for IT. The processing power of a quantum system expands exponentially with each additional qubit. Arranging the interference between the amplitudes of a multi-qubit processor in various ways unlocks solutions to computational tasks that are impossible for even the most powerful classical supercomputer to achieve. 

In classical physics, we observe systems passively. We can, for example, watch a person kick a ball without detection or influencing the action. Such is not the case for quantum. It is impossible to observe quantum information without interfering or leaving behind evidence.

Moreover, entangled qubits can exist in states that cannot be factored in. The majority of quantum states involve entanglement, thus phenomenon is critical for quantum processing. Because entangled qubits do not need to be in the same location, entanglement opens up a host of communication technology opportunities.

These and other examples demonstrate quantum’s immense potential for computer processing, cryptography, secure communication, and more.

Types of quantum information technology

Quantum computing

Quantum computers represent a groundbreaking paradigm in computation, harnessing the principles of quantum mechanics to perform calculations at unparalleled speeds. Central to their operation are qubits, the quantum counterparts to classical bits, which exploit the phenomena of superposition and entanglement to encode and process information in fundamentally different ways.

Superposition enables qubits to exist in multiple states at one time, offering the potential for exponential parallelism in computation. Meanwhile, entanglement establishes correlations between qubits that defy classical intuition, enabling the creation of highly correlated states that encode and manipulate quantum information with extraordinary efficiency.

Through the phenomenon of interference, where the probability amplitudes of different quantum states interfere with one another, quantum computers can exploit the computational advantages of superposition and entanglement to perform complex computations. This method leads to potential speedups for specific computational tasks, such as integer factorization with Shor’s algorithm and unstructured search with Grover’s algorithm.

Quantum computers hold immense promise for artificial intelligence, cryptography, materials science, optimization, and other fields. However, realizing this potential requires overcoming significant challenges, such as decoherence, noise, and the engineering of scalable quantum hardware.

Despite these hurdles, ongoing research and development efforts are advancing the capabilities of quantum computing systems. As progress continues, we anticipate the emergence of increasingly powerful and versatile quantum computers that push the boundaries of what is computationally achievable, revolutionizing the computing landscape as we know it.

Quantum sensing

Quantum sensing is a cutting-edge technology that uses the principles of quantum mechanics to achieve ultra-high-precision measurements beyond the capabilities of classical sensors. At its core, quantum sensing exploits quantum properties such as superposition and entanglement to enhance measurement sensitivity and accuracy.

Highly precise atomic clocks are a prominent example of quantum sensing. Atomic clocks rely on the quantum properties of atoms, typically cesium or rubidium, to measure time with extraordinary accuracy. By leveraging the precise frequency of atomic transitions, atomic clocks maintain timekeeping accuracy at the level of nanoseconds over periods of millions of years.

Another key application of quantum sensing is quantum magnetometry, which aims to detect and measure magnetic fields with unprecedented sensitivity. Quantum magnetometers use the quantum properties of atomic spins to sense minute changes in magnetic fields. Quantum magnetometry has applications in various fields, including geophysics, navigation, and medical imaging, where high-precision magnetic field measurements are crucial.

Additionally, quantum sensors are under development for other applications, such as gravity sensing, inertial sensing, and quantum imaging. Quantum gravity sensors, for example, aim to detect tiny variations in gravitational fields, offering insights into geological structures, underground resources, and environmental changes. Inertial sensors based on quantum technology could revolutionize navigation systems by providing precise positioning and orientation information in GPS-denied environments.

Advancements in quantum technologies, including qubit control, quantum measurement techniques, and quantum error correction, are driving the development of quantum sensors. These developments enable the creation of sensors with unprecedented sensitivity, precision, and robustness, opening up new opportunities for scientific research, industrial applications, and technological innovation.

Overall, quantum sensing holds the promise of transforming fields such as geophysics, navigation, medical diagnostics, and environmental monitoring by providing ultra-high-precision measurements unattainable with classical sensors. As research and development into quantum sensing advances, we can expect to see even greater strides in precision measurement technology, leading to new insights and discoveries across various domains.

Quantum communication

Quantum communication is an emerging field that uses quantum mechanics principles to secure the transmission of information between parties. Unlike classical communication protocols, which rely on mathematical algorithms for encryption, quantum communication protocols leverage the inherent properties of quantum systems to achieve unbreakable security.

At the heart of quantum communication lies the phenomenon of quantum entanglement. In this concept, the states of two or more particles become correlated so that the state of one particle immediately influences the state of another, regardless of how far apart they are.

A leading quantum communication application is quantum key distribution (QKD), which enables the generation of cryptographic keys with unconditional security. In a typical QKD protocol, two parties, often referred to as Alice and Bob, exchange quantum states encoded with random information. Any attempt to intercept or measure these quantum states would disturb them, revealing the presence of the eavesdropper, often called Eve, to Alice and Bob.

The laws of quantum mechanics, specifically the no-cloning theorem and the principle of quantum indeterminacy, guarantee QKD protocol security. These principles ensure that any attempt to measure or copy the quantum states without detection results in irreversible disturbance, thereby preventing eavesdropping without detection.

Beyond QKD, quantum communication encompasses other cryptographic protocols, such as quantum teleportation, quantum digital signatures, and quantum coin flipping. These protocols leverage the unique properties of quantum systems, including superposition and entanglement, to enable secure communication and authentication between parties.

Quantum communication technologies are still in the early stages of development, but they hold immense promise for applications requiring secure and private communication, such as banking, government communications, and military operations. As research and development into quantum communication advances, expect to see increasingly sophisticated and practical implementations of quantum communication protocols, ushering in a new era of secure communication in the digital age.

Advantages of QIT for industry

Want help or have questions?

Worldwide