Können wir Ihnen behilflich sein?
E7515W UXM Wireless Connectivity Test Platform for Wi-Fi®
Press Kit
Press Release
Media Presentation
E7515W UXM Wireless Connectivity Test Platform Overview
Keysight Offers Complete Development Ecosystems Across the Wireless Industry
Video
E7515W UXM Wireless Connectivity Test Platform Spotlight
The new Keysight E7515W UXM Wireless Connectivity Test Platform extends the UXM Platform – the world’s most powerful 5G network emulator – to support extensive Wi-Fi testing. This system performs Wi-Fi RF to Application, and Wi-Fi to Cellular interworking testing of both Wi-Fi clients (STAs) and Access Points.
Image Library
White Paper
Everything You Need to Know About Wi-Fi® 7
Consumer demand for wireless data access and throughput has grown steadily since wireless local area networks (WLAN) first became popular with the adoption of the Institute of Electrical and Electronics Engineers (IEEE) 802.11 standard in 1997. Today, users expect widespread availability of high-speed WLAN to support data-intensive applications. WLAN-enabled devices sharing a network have also significantly increased as PCs, smartphones, tablets, cameras, TVs, and smart home devices increase at home.
Media Contacts
Contacts
Paul Erwin, Americas/Europe
+1 248 430–9075
[email protected]
Fusako Dohi, Asia
+81 42 660–2162
[email protected]
Jenny Gallacher, Europe
+44 (0) 7800 737–982
[email protected]
Additional Information
More information is available at E7515W UXM Wireless Connectivity Test Platform for Wi-Fi®.
Need to contact Media Relations at Keysight?