Können wir Ihnen behilflich sein?
Keysight Expands Novus Portfolio with Compact Automotive Software Defined Vehicle Test Solution
- Enables network engineers to test performance and conformance of software-defined vehicles on a single platform with traffic generation and protocol testing capabilities
- Provides time-sensitive networking and compliance testing for automotive Ethernet, vital for safety in advanced driver-assistance systems and autonomous vehicles
- Protects critical systems, improves reliability, and enhances data security with comprehensive 802.1AE Layer-2 MACsec security and protocol testing
SANTA ROSA, Calif. January 07, 2025
Keysight Technologies, Inc. (NYSE: KEYS) announces the expansion of its Novus portfolio with the Novus mini automotive, a quiet small form-factor pluggable (SFP) network test platform that addresses the needs of automotive network engineers as they deploy software-defined vehicles (SDV). Keysight is expanding the capability of the Novus platform by offering a next-generation vehicle interface that includes 10BASE-T1S, and multi-gigabyte BASE-T1 support for 100 megabytes per second, 2.5 gigabits per second (Gbit/s), 5Gbit/s, and 10Gbit/s. Keysight’s SFP architecture provides a flexible platform to mix and match speeds for each port with modules plugging into existing cards rather than requiring a separate card, as many current test solutions necessitate.
As vehicles move to zonal architectures, connected devices are a critical operational component. As a result, any system failures caused by connectivity and network issues can impact safety and potentially create life-threatening situations. To mitigate this risk, engineers must thoroughly test the conformance and performance of every system element before deploying them.
Key benefits of the Novus mini automotive platform include:
- Streamlines testing – The combined solution offers both traffic generation and protocol testing on one platform. With both functions on a single platform, engineers can optimize the testing process, save time, and simplify workflows without requiring multiple tools. It also accelerates troubleshooting and facilitates efficient remediation of issues.
- Helps lower costs and simplify wiring – Supports native automotive interfaces BASE-T1 and BASE-T1S that help lower costs and simplify wiring for automotive manufacturers, reducing the amount of required cabling and connectors. BASE-T1 and BASE-T1S offer a scalable and flexible single-pair Ethernet solution that can adapt to different vehicle models and configurations. These interfaces support higher data rates compared to traditional automotive communication protocols for faster, more efficient data transmission as vehicles become more connected.
- Compact, quiet, and affordable – Features the smallest footprint in the industry with outstanding cost per port, and ultra-quiet, fan-less operation.
- Validates layers 2–7 in complex automotive networks – Provides comprehensive performance and conformance testing that covers everything from data link and network protocols to transport, session, presentation, and application layers. Validating the interoperability of disparate components across layers is necessary in complex automotive networks where multiple systems must seamlessly work together.
- Protects networks from unauthorized access – Supports full line rate and automated conformance testing for TSN 802.1AS 2011/2020, 802.1Qbv, 802.1Qav, 802.1CB, and 802.1Qci. The platform tests critical timing standards for automotive networking, as precise timing and synchronization are crucial for the reliable and safe operation of ADAS and autonomous vehicle technologies. Standards like 802.1Qci help protect networks from unauthorized access and faulty or unsecure devices.
Ram Periakaruppan, Vice President and General Manager, Network Test & Security Solutions, Keysight, said: "The Novus mini automotive provides real-world validation and automated conformance testing for the next generation of software defined vehicles. Our customers must trust that their products consistently meet quality standards and comply with regulatory requirements to avoid costly fines and penalties. The Novus mini allows us to deliver this confident assurance with a compact, integrated network test solution that can keep pace with constant innovation.”
Keysight will demonstrate its portfolio of test solutions for automotive networks, including the Novus mini automotive, at the Consumer Technology Show (CES), January 7-10th in Las Vegas, NV, West Hall, booth 4664 (Inside the Intrepid Controls booth).
Resources
- Product page: Keysight Novus mini automotive
- Product page: Novus Load Module Portfolio
- Data sheet: Novus mini
About Keysight Technologies
At Keysight (NYSE: KEYS), we inspire and empower innovators to bring world-changing technologies to life. As an S&P 500 company, we're delivering market-leading design, emulation, and test solutions to help engineers develop and deploy faster, with less risk, throughout the entire product life cycle. We're a global innovation partner enabling customers in communications, industrial automation, aerospace and defense, automotive, semiconductor, and general electronics markets to accelerate innovation to connect and secure the world. Learn more at Keysight Newsroom and www.keysight.com.
Contacts
North America PR Team
[email protected]
Fusako Dohi, Asia
+81 42 660–2162
[email protected]
Jenny Gallacher, Europe
+44 118 927 4003
[email protected]
Need to contact Media Relations at Keysight?