Keysight’s 5G Test Platforms Used to Establish the Industry’s First 5G New Radio Data Connection Based on 3GPP Release 16

Qualcomm Technologies, Inc. validates 5G new radio Rel-16 chipset using Keysight’s 5G Protocol R&D Toolset

SANTA ROSA, Calif., February 17, 2021

Keysight Technologies, Inc. (NYSE: KEYS), a leading technology company that helps enterprises, service providers and governments accelerate innovation to connect and secure the world, announced that company's 5G test solutions were used to establish the industry's first 5G new radio (NR) data connection based on 3GPP Release 16 specifications (Rel-16).

3GPP Rel-16 introduces new capabilities, including ultra-reliable and low latency communications (URLLC). When combined with network slicing, these capabilities support enterprises, industrial internet of things (IIoT) applications and private 5G deployments. The new release also helps public safety organizations deliver advanced mission critical services and the automotive industry integrate advanced connectivity features in vehicles and infrastructure, making transportation efficient and roads safer.

Keysight's 5G Protocol R&D Toolset, part of the company's suite of network emulation solutions, enables wireless leaders such as Qualcomm Technologies and device vendors validate designs based on 3GPP Rel-16.

"Keysight is helping 5G device makers to confidently deliver products based on the latest 3GPP 5G new radio standard, which will unlock many new 5G opportunities beyond traditional mobile broadband services," said Mosaab Abughalib, senior director, engineering at Keysight Technologies. "Establishing the industry's first 5G data connection based on 3GPP Rel-16 enables chipset and device vendors to take full advantage of 5G NR, resulting in improved efficiencies in transportation, logistics and manufacturing, as well as providing better cell coverage and connection speeds for consumers."

Keysight's Protocol R&D Toolset enables chipset and device manufacturers to seamlessly prototype designs using tests that verify 5G NR signaling protocols. With full access to testing parameters across layer one, two and three, the Protocol R&D Toolset allows developers to flexibly create and execute test cases, debug errors and fully analyze results in sub-7GHz and mmWave spectrum, for both non-standalone (NSA) and standalone (SA) mode.

About Keysight Technologies

Keysight Technologies, Inc. (NYSE: KEYS) is a leading technology company that helps enterprises, service providers and governments accelerate innovation to connect and secure the world. Keysight's solutions optimize networks and bring electronic products to market faster and at a lower cost with offerings from design simulation, to prototype validation, to manufacturing test, to optimization in networks and cloud environments. Customers span the worldwide communications ecosystem, aerospace and defense, automotive, energy, semiconductor and general electronics end markets. Keysight generated revenues of $4.2B in fiscal year 2020. More information is available at www.keysight.com.

# # #

Additional information about Keysight Technologies is available in the newsroom at https://www.keysight.com/go/news and on Facebook, LinkedIn, Twitter, and YouTube.

Keysight Contact:

Geri Lynne LaCombe, Americas/Europe
+1 303 662–4748
geri_lacombe@keysight.com

Fusako Dohi, Asia
+81 42 660–2162
fusako_dohi@keysight.com

Netherlands