Used Equipment Store

Account Benefits

Get a customised view of the Used Equipment Store

Manage your details to get quick responses by the team

Stay up-to-date on specials, prices and availability

Already have an account? Log In

Create Your Account

Sign up to receive marketing or promotional emails from Keysight

By submitting this form, you are providing Keysight with your personal data. For information on how we use this data, see the Keysight Privacy Statement.

Engineer's Toolkit: Understanding Arbitrary Waveform Generators vs Function Generators

Your browser limits use of the Used Keysight Equipment website.
Please consider switching to a current version of Chrome, Firefox, Edge or IE11 to use this site.

Do you find yourself grappling with the complexities of signal generation for intricate circuit designs and system validation? Waveform generation plays a pivotal role in the testing and development phases of modern electronics. 

In today's rapidly evolving tech landscape, the choice of waveform generators can make or break your testing and development process. 

Essential to every electrical engineer's toolkit, waveform generators, arbitrary waveform generators (AWGs) and function generators—serve as crucial enablers for meticulous and effective testing.

Basics and Evolution of Waveform Generation

Waveform generation, at its core, involves the synthesis of electrical waveforms that simulate various conditions a system might encounter. From basic sine waves to complex, modulated signals, waveform generators have proven to be indispensable tools in electrical engineering. 

They offer engineers the means to develop, test, and debug circuits, devices, and systems by replicating real-world conditions or creating theoretically possible but yet-unobserved scenarios.

In the earlier years of electronic development, engineers relied heavily on oscillators and function generators that produced basic waveforms like sine, square, and triangle waves. They were relatively simple but did the job for the rudimentary electronics of the time. 

Fast forward to the late 20th century, and we see the introduction of digital signal processors (DSPs) and microcontrollers, elevating the precision and capabilities of waveform generators.

Today, AWGs represent the pinnacle of flexibility in waveform generation. They enable the creation of any mathematically describable waveform and allow for amplitude, frequency, and phase modulation, among other things. 

On the other hand, function generators remain relevant for their ease of use and aptness for basic testing needs.

Understanding the capabilities and limitations of each type of waveform generator allows for informed decision-making tailored to the specific demands of your project. 

Whether you are designing a state-of-the-art communication system or troubleshooting a simple analog circuit, the right waveform generator proves to be an invaluable asset.

What is a Function Generator?

A function generator is a specific type of signal generator that produces various standard waveforms over a wide range of frequencies. It primarily serves as a reliable tool for testing and simulating signals in electrical and electronic circuits.

Main Features of Function Generators

  • Standard waveforms: Generates basic waveforms like sine, square, and triangle waves.
  • Frequency range: Typically operates over a range from less than 1Hz to several MHz.
  • Amplitude control: Allows adjustment of the amplitude or peak-to-peak voltage of the output signal.
  • Phase modulation: Offers basic phase shift capabilities, although usually less extensive than those found in AWGs.
  • Sweep functionality: Can vary frequency over time, useful for frequency response testing.

Typical Uses:

  • Electrical signal simulation for basic circuit analysis
  • Frequency response testing of audio equipment
  • Basic modulation experiments
  • Troubleshooting electrical systems

Technical Specifications to Consider:

  • Frequency range: Make sure it covers the frequencies essential for your project.
  • Output impedance: Usually 50 ohms, should match with your testing setup.
  • Harmonic distortion: Lower values indicate a cleaner signal.
  • User interface: Check if it's intuitive and matches your workflow.
  • Additional features: Such as built-in counters or digital displays.

When choosing a function generator, consider the scope and precision demands of your project. Function generators shine in user-friendliness, cost-effectiveness, and quick setup, making them ideal choices for less complex projects or educational settings. 

However, they come with constraints, such as limited flexibility in waveform generation and reduced precision at higher frequencies. These limitations may push you toward an upgrade to an arbitrary waveform generator for tasks that require greater flexibility and higher resolution.

Find Function Generators On Sale: Precision at Your Fingertips

  • Like-new Condition
  • Updated Firmware
  • Full Calibration
  • New Accessories
  • Like-new Warranty
  • Customization possible

Learn more

  • Savings of up to 90%
  • Working Condition
  • Calibrated or Tested
  • 30-Day Right-of-Return
  • No Customization
  • Shipping to limited countries

Learn more

Second-Hand. First-Class.

Great savings that come with a worry-free, first-class experience. That’s what buying used equipment directly from Keysight is all about!

Why You Should
Work with Keysight
Up to 5 years
warranty
Add Hardware.
Enhance Software.
Personalized Service,
Local Team
Empowering Innovators
for 80+ Years
Save 40-90% on
Used Equipment
Latest Firmware
and Calibration

Select up to 3 instruments to compare

Cancel
Select another instrument to compare
Starting at
Select another instrument to compare
Starting at
Select another instrument to compare
Starting at

Enable Notifications

In order to use this feature, you need to enable notifications.

Manage notification preferences

USD


What is an Arbitrary Waveform Generator?

An arbitrary waveform generator (AWG) is a sophisticated type of signal generator that can generate arbitrary waveforms defined by a sequence of data points. 

Unlike function generators that are restricted to standard waveforms, AWGs offer greater flexibility and control, allowing you to replicate almost any conceivable waveform.

Distinguishing Features of AWGs

  • Custom waveform creation: Ability to generate user-defined waveforms.
  • High precision: Offers greater accuracy and resolution compared to most function generators.
  • Modulation capabilities: Supports a wide variety of modulation types, including AM, FM, and phase modulation.
  • Multiple channels: Many models come with multiple output channels, enabling complex signal scenarios.
  • Integrated memory: Allows the storage of predefined waveforms for quick recall.

Common Scenarios Where AWGs Shine:

  • Advanced research and development projects
  • Complex modulation schemes in telecommunications
  • Signal impairment simulations
  • Calibration and equipment validation in high-precision settings

Technical Specifications to Consider:

  • Sample rate: Determines the maximum frequency and resolution of the generated waveform.
  • Waveform memory depth: More memory allows for longer and more complex waveforms.
  • Output range: Check both the amplitude and frequency ranges.
  • Connectivity: Options like USB, Ethernet, and GPIB for remote control and data transfer.
  • Channel count: Depending on your needs, you might require multiple output channels.

AWGs offer unparalleled flexibility and precision, making them essential tools for complex, high-stakes projects. They excel in scenarios that require custom waveform generation, advanced modulation schemes, or high-resolution signals. However, this level of sophistication comes at a cost, both financially and in terms of user complexity.

AWGs are generally more expensive and may require a steeper learning curve compared to function generators. Thus, while they offer more advanced features, you'll need to weigh these against the higher costs and potentially more complex operation.

Find Arbitrary Waveform Generator On Sale Now

  • Like-new Condition
  • Updated Firmware
  • Full Calibration
  • New Accessories
  • Like-new Warranty
  • Customization possible

Learn more

  • Savings of up to 90%
  • Working Condition
  • Calibrated or Tested
  • 30-Day Right-of-Return
  • No Customization
  • Shipping to limited countries

Learn more

FAQs

Get answers to Frequently Asked Questions about Shipping, Payment, Quote Processes, Pricing, Stores, etc.

Why You Should
Work with Keysight
Up to 5 years
warranty
Add Hardware.
Enhance Software.
Personalized Service,
Local Team
Empowering Innovators
for 80+ Years
Save 40-90% on
Used Equipment
Latest Firmware
and Calibration

Select up to 3 instruments to compare

Cancel
Select another instrument to compare
Starting at
Select another instrument to compare
Starting at
Select another instrument to compare
Starting at

Enable Notifications

In order to use this feature, you need to enable notifications.

Manage notification preferences

USD


Side-by-Side Comparison: AWG vs Function Generator

For an electrical engineer, the choice between an arbitrary waveform generator (AWG) and a function generator can influence the quality of research, testing, and development efforts. Both have unique features that make them well-suited for particular applications. 

Below is a table that details the key attributes of both types of waveform generators, designed to offer engineers a quick but comprehensive understanding of their differences and similarities.

AttributeArbitrary Waveform Generator (AWG)Function Generator
Waveform TypesCustom, user-defined waveformsStandard (Sine, Square, Triangle)
PrecisionHighModerate to Low
Frequency RangeUsually higher, up to GHzUp to several MHz
Modulation CapabilitiesExtensive (AM, FM, PM and more)Limited (mostly AM and FM)
ChannelsMultiple Channels CommonUsually Single Channel
CostHighModerate to Low
User ComplexitySteeper learning curveEasier to use
MemoryIntegrated, larger storageLimited or None
Output RangeWider amplitude and frequency rangesMore restricted
ConnectivityUSB, Ethernet, GPIBUsually USB or none

Comprehensive Overview

Arbitrary Waveform Generators (AWGs)
AWGs stand out when you need to generate custom waveforms or require high-precision signals. They are particularly useful in complex modulation scenarios like in advanced telecommunications or in scientific research where the ability to simulate arbitrary signals is invaluable. 

Their multiple channels enable the generation of complex signal scenarios, perfect for intricate system validations. However, AWGs can be costly and may present a steep learning curve.
Function Generators
Function generators are the go-to devices for simpler tasks that require basic waveforms like sine, square, or triangle. 

They are easier to use, usually cheaper, and generally quicker to set up, making them ideal for basic tests, educational purposes, and lower-budget projects. 

However, they often lack the precision and flexibility provided by AWGs, particularly in generating non-standard waveforms and handling advanced modulation schemes.

Choosing between an AWG and a function generator hinges on several factors—most notably, the complexity of your application, your budget, and your proficiency with the equipment. 

Function generators suit projects that require standard waveforms and minimal setup time but may fall short in terms of accuracy and customizability. 

On the other hand, if your project demands high precision, complex waveforms, or advanced modulation capabilities, an AWG is undoubtedly the better option, provided you are prepared for its higher cost and complexity.

Real-world Applications and Recommendations

When to Choose a Function Generator
Function Generators often find applications in scenarios requiring straightforward, basic testing. For example, they are immensely useful in educational settings for teaching the fundamentals of waveforms and signal analysis. 

They're also ideal for basic electronics repair shops to test component functionality. In audio engineering, a function generator can quickly test the frequency response of speakers or other audio equipment. Simplicity, quick setup, and lower cost make function generators the go-to in these cases.

When to Opt for an Arbitrary Waveform Generator (AWG)
AWGs are indispensable in cutting-edge research and development environments. Telecommunications companies frequently use them to test new modulation schemes for higher data rates or better signal quality. 

In automotive applications, AWGs can simulate complex signals such as those found in sophisticated sensor arrays. Additionally, in quantum computing research, AWGs generate the precise waveforms needed to manipulate quantum bits. 

When the task demands high accuracy, flexibility, and the ability to generate custom waveforms, AWGs are the tool of choice.

Advice Based on Applications:

  1. Educational labs: Function generators suffice for most educational applications.
  2. Advanced R&D: AWGs offer the versatility and precision required.
  3. Audio engineering: A function generator usually suffices, but an AWG may be necessary for high-precision work.
  4. Telecommunications: AWGs are almost mandatory for simulating complex modulations and encoding schemes.

Integration with Other Tools

Function generators generally offer fewer connectivity options, but their simplicity makes them relatively easy to integrate with other basic testing equipment like oscilloscopes. Many have BNC connectors for quick hookup to commonly used tools.

AWGs usually come with a range of connectivity options like USB, Ethernet, and GPIB, allowing for more seamless integration into automated test setups and high-end measurement systems. They can often interface directly with software tools for advanced data analysis and are better suited for setups that include equipment like high-precision oscilloscopes or signal analyzers.

Ultimately, the choice between a function generator and an AWG depends on the specific needs of your application. While function generators cover the basics efficiently and at a lower cost, AWGs offer unparalleled flexibility and precision—albeit at a higher price point and with a steeper learning curve. 

Choose the one that aligns most closely with your project requirements, complexity, and budget.

Safety and Calibration Essentials

The importance of using calibrated equipment in waveform generation cannot be overstated. Accurate and reliable measurements are crucial for the success of any testing or development project. 

The lack of calibration can lead to inaccurate data, making your results unreliable and potentially causing costly errors in the long run.

Universal Safety Guidelines:

  1. Turn off equipment: Always turn off and unplug the equipment when making any internal adjustments or connections.
  2. Check ratings: Make sure the voltage and current ratings of your testing setup match the capabilities of your waveform generator.
  3. Use proper cables: Use shielded cables and connectors that meet the specifications for your particular application.
  4. Follow manufacturer guidelines: Always consult the user manual for specific safety precautions unique to your device.

Keysight Instrument Calibration

Keysight takes calibration seriously, ensuring that "we measure every specification, every option, every time." 

Whether you're using an AWG or a function generator, you can select the standard compliance that best meets your test strategy.

Depending on your needs, Keysight offers a range of calibration services:

  • Measurement uncertainties: For those requiring a high level of accuracy.
  • Guardbanding: For extra safety margins.
  • Accredited calibration: Meets stringent international standards.
  • Primary standards lab calibration: For the most demanding accuracy requirements.

Additionally, Keysight tailors its calibration reports to meet specific metrology standards, including ISO 17025:2005 and ANSI Z540.3-2006, providing a wide range of options to meet both local and global needs. 

All Keysight service centers hold accreditations from local bodies such as JCSS, CNAS, Poverka, UKAS, ANAB, and many more, ensuring that your ANSI Z540.3-2006 equipment meets the highest quality standards.

Proper calibration and adherence to safety guidelines are not just best practices; they are necessities. Always opt for accredited calibration services like those offered by Keysight to ensure the most accurate and reliable performance from your waveform generators.

Expert Insights: Making the Right Choice for Your Project

Choosing between an arbitrary waveform generator and a function generator involves a nuanced understanding of your project's specific needs, your budget constraints, and the results you aim to achieve. 

Here's how to make an informed decision:

Nature of the Project:

  • Simple testing and education: If your project involves basic testing scenarios or is educational in nature, a function generator often suffices. It provides standard waveforms like sine, square, and triangle, and is straightforward to operate.
  • Complex scenarios: If your project demands the simulation of complex, real-world scenarios, custom waveforms, or a high level of precision, an AWG becomes a necessity. The ability to generate user-defined waveforms allows for more complex testing and research scenarios.

Budget Considerations:

  • Cost-effectiveness: Function generators are usually more budget-friendly and offer good value for straightforward applications.
  • High investment: AWGs come at a premium but offer a broader range of features and capabilities, justified in projects that demand high precision and flexibility.

Desired Outcomes:

  • Quick and basic: If your goal is quick verification or testing of components, a function generator usually gets the job done effectively and quickly.
  • Advanced and detailed: For tasks that require extensive data analysis or high-accuracy results, an AWG offers the level of detail and customizability that you'll need.

Think about the lifecycle of your project and any future tasks that might arise. Sometimes investing in an AWG upfront can save costs in the long run, especially if your project is likely to evolve into something more complex. 

Always weigh the immediate needs against future requirements, and consider the total cost of ownership, not just the initial investment.

Conclusion: Equipping Yourself for Success in Electrical Engineering

Navigating the complexities of modern electrical engineering projects demands tools that are not just powerful but also precisely suited to your specific needs. 

The choice between an arbitrary waveform generator and a function generator is not merely a technical decision; it's a strategic one that can significantly impact the quality and success of your work. 

By understanding the differences and strengths of each type of waveform generator, you equip yourself with the capability to tackle a broad range of applications—from simple component testing to groundbreaking research and development.

The right waveform generator can be your invaluable partner in innovation, enabling you to push the boundaries of what's possible in electrical engineering. 

Whether you're shaping the future of telecommunications, pioneering advances in scientific research, or simply teaching the next generation of engineers, your choice of waveform generator can either limit you or empower you. 

Make that choice wisely; your project's success could depend on it.

Whenever You’re Ready, Here Are 5 Ways We Can Help You

  1. Browse our premium used network analyzers, oscilloscopes, signal analyzers and waveform generators.
  2. Call tech support US: 1 800 829-4444
    Press #, then 2. Hours: 7am – 5pm MT, Mon– Fri
  3. Talk to our sales support team by clicking the icon (bottom right corner) on every offer page
  4. Create an account to get price alerts and access to exclusive waitlists
  5. Talk to your account manager about your specific needs.

Subscribe to Get Our Latest News, Updates, and Articles.

Get Email Updates

* Two weeks shipping time offer available for US customers only. Dependent on item availability and location