The future of the automotive industry relies on the electronic revolution and integration with the clean energy ecosystem. Dramatic increases in the number of sensors and applications mean new tests are needed for power efficiency, secure, reliable connections, and sensor fusion. Accelerate your automotive innovations today by thoroughly validating your vehicle systems to ensure reliability, conformance to standards, as well as safety.

NEXT-GENERATION AUTOMOTIVE RADAR

From radar and cameras to lidar, sensor technologies coupled with powerful artificial intelligence (AI) software will enable all levels of advanced driver assistance systems (ADAS) and make self-driving vehicles a reality.

Your designers and engineers need to prove that their mission-critical systems are perfectly safe. They can validate and demonstrate accuracy and dependability with our simulation and test solutions.

Accelerate the Automotive Revolution

AUTO MAKER SPEEDS UP DEVELOPMENT WITH RADAR MODELING

A major global automotive manufacturer develops advanced driver assistance systems with high-frequency, high-bandwidth radar sensors. Using the SystemVue Automotive Radar Library software with the M8195A arbitrary waveform generator and the N9041B UXA signal analyzer, they reduced development time by up to 30%. The manufacturer realized an estimated 20% design time savings by enabling engineers to verify and address problems much earlier in the design process.

Want to leverage Keysight eMobility and Connected Car Expertise?