Keysight Delivers USB4TM Version 2.0 Solutions to Optimize Design Performance and Ensure Standards Compliance

New solution suite enables customers to develop and validate USB interfaces for new USB 80Gpbs implementations quickly and accurately

SANTA ROSA, Calif., November 8, 2022 

Keysight Technologies, Inc. (NYSE: KEYS), a leading technology company that delivers advanced design and validation solutions to help accelerate innovation to connect and secure the world, announced a new set of USB 80Gbps solutions that maximize the performance of USB designs and ensure compliance with the specifications implemented by the USB Implementers Forum (USB-IF) standard to deliver accuracy and high signal fidelity.  

A wide range of products, including smartphones, laptops, desktop computers, tablets, and digital cameras rely on next-generation high-speed digital standards. USB 80Gbps, a plug and play interface for inter-digital communication, provides significant advantages in bandwidth and data delivery.

Keysight offers a set of new USB 80Gbps solutions to enable customers to design, debug, and test their technologies, including:

In accordance with the USB standard and to ensure the interoperability of USB devices, Keysight offers a comprehensive portfolio of high-speed digital instrumentation including:

  • UXR real-time oscilloscope, providing accuracy in waveform representation across a wide frequency range
  • Highly integrated Bit Error Ratio Testers (BERTs), which identify errors introduced into the system when data is received – a critical capability in physical layer characterization, validation, and compliance testing
  • Vector Network Analyzers, which measure the amplitude and phase responses caused by a device, where the resulting transmission and reflection measurements, impedance, and s-parameters are then used for compliance tests and characterization

John Koeter, Senior Vice President of Marketing and Strategy for the Solutions Group at Synopsys, said: “USB4 is the ubiquitous standard for secure, seamless connectivity of high-definition displays and high-throughput peripherals requiring speeds of up to 80Gbps. Synopsys USB controller, PHY and verification IP solutions leverage Keysight’s design and validation technologies to ensure robustness and compliance of the IP at maximum speeds, enabling designers to quickly deliver interoperable products with less risk.”

Joachim Peerlings, Vice President and General Manager of Keysight’s Network and Data Center Solutions Group, said: “With the proliferation of 5G and billions of connected devices, data center operators and device makers need ways to ensure data throughput demands meet cost, performance, and power targets. We’re proud to enable faster and risk-free interoperability and compliance of devices using high-speed interfaces like USB 80Gbps”.

About Keysight Technologies   

Keysight delivers advanced design and validation solutions that help accelerate innovation to connect and secure the world. Keysight's dedication to speed and precision extends to software-driven insights and analytics that bring tomorrow's technology products to market faster across the development lifecycle, in design simulation, prototype validation, automated software testing, manufacturing analysis, and network performance optimization and visibility in enterprise, service provider and cloud environments. Our customers span the worldwide communications and industrial ecosystems, aerospace and defense, automotive, energy, semiconductor and general electronics markets. Keysight generated revenues of $4.9B in fiscal year 2021. For more information about Keysight Technologies (NYSE: KEYS), visit us at www.keysight.com.

# # #

Additional information about Keysight Technologies is available in the newsroom at https://www.keysight.com/go/news and on Facebook, LinkedIn, Twitter, and YouTube.

Keysight Contact:

Geri Lynne LaCombe, Americas/Europe
+1 303 662–4748
geri_lacombe@keysight.com

Fusako Dohi, Asia
+81 42 660–2162
fusako_dohi@keysight.com

Keysight’s D9050USBC Transmitter Test Application

Schweiz