Media Advisory 

Keysight to Showcase Solutions that Accelerate Radio Frequency Innovation at EuMW23

SANTA ROSA, Calif. September 6, 2023 

 

What: At EuMW 2023, Keysight will be showcasing solutions that accelerate radio frequency (RF) innovation for applications from space and automotive to 5G / 6G and internet of things (IoT). As a 20-year consecutive Platinum sponsor of EuMW, Keysight is enabling innovators to push the engineering boundaries by quickly solving the design, emulation, and test challenges of RF, millimeter wave, and more.

When: September 17-22, 2023

Where: Keysight Booth #107A
Messe Berlin hub27
Berlin, Germany

Media: Contact Paul Erwin to schedule media briefings and solution demonstrations.

Info: Keysight at European Microwave Week

 

Keysight experts will be demonstrating: 

System performance modeling: This demonstration compares predicted performance from the newly released Keysight PathWave System Design 2024 predicted against the physical-world measurements. Includes predicting true end-to-end system performance inclusive of kinematics and RF impairments and introduces hardware-in-the-loop to enable concurrent engineering at the subsystem level.

mmWave circuit design: Keysight's new PathWave ADS 2024 software offers breakthrough 3D electromagnetic (EM) circuit physical co-design and verification for today's challenging 5G monolithic microwave integrated circuits (MMICs) and modules. The solution extends its open, multi-technology workflows and enterprise-scale and Python automation to enable today's digital transformation with leadership technology to pioneer your pre-6G and sub-THz research. Visit us for a demo of the latest tools for microwave power amplifier designs that address innovative analysis around electrothermal, load pull, and digital pre-distortion (DPD).

Wideband MIMO prototyping: Multiple-input / multiple-output (MIMO) will be a key enabler for 6G to achieve data throughputs of > 100 Gbps using multiple streams of data with 10 to 30 GHz of bandwidth at sub-THz frequencies. Keysight demonstrates solutions providing flexibility and scalability in prototyping various types of waveforms operating in different frequency bands.

Modulate with confidence: The demand for faster data rates is driving the use of increased bandwidths and more complex modulation schemes. This demonstration showcases the latest test solutions from Keysight, delivering low-distortion signals with high-order modulation up to 4096 QAM to the device-under-test (DUT), giving better insight into the true performance of your device.

Phase noise measurement: Demonstrates how component and circuit designers can easily characterize signal sources with a simple setup and achieve stable voltage-controlled oscillator (VCO) measurements. Keysight's solution can measure low-phase noise more accurately than conventional instruments using cross-correlation to provide better measurement sensitivity.

Automotive radar test: Showcases how Keysight's new Automotive Radar E-Band mixer simplifies automotive radar test setups, integrates receiver and transmitter capability, and enables MIMO testing. Learn how to analyze and generate automotive radar signals with scalable analysis bandwidth across the full frequency range.

Test PA modules 50% faster: Demonstrates the new Keysight E5081A ENA-X, which enables multiple measurement parameters with a single connection, including noise figure, EVM, adjacent channel power ratio (ACPR), and standard S-parameters. Covers a spectral correlation technique that directly analyzes the modulated input and output signals in the frequency domain while applying full vector correction at the device under test (DUT) plane.

Phased array evaluation: Showcases the Keysight phased array calibration and test solution provides a convenient user interface for fast, automated phased array calibration and beamforming performance verification within an over-the-air (OTA) test environment. Learn how the solution takes test times from minutes to seconds without compromising accuracy.

Sub-THz device analysis: While 6G deployment in sub-THz may be a few years away, researchers are already beginning to build out the components necessary to enable the sub-THz ecosystem. Learn how the Keysight Vector Component Analyzer (VCA) solution enables engineers to minimize the residual error vector magnitude (EVM) of the test system and zero in on component performance.

Field spectrum audit: Demonstration of Keysight's new FieldFox C-model handheld analyzer offers fully upgradable frequency and bandwidth plus over 20 software applications. This solution is the first in the industry to provide over the air, end-to-end troubleshooting and network auditing to help operators efficiently manage networks. Showcases signal and protocol sniffing that provide end-to-end full-stack network troubleshooting capability to improve 5G network deployment efficiency.

About Keysight Technologies   

At Keysight (NYSE: KEYS), we inspire and empower innovators to bring world-changing technologies to life. As an S&P 500 company, we're delivering market-leading design, emulation, and test solutions to help engineers develop and deploy faster, with less risk, throughout the entire product lifecycle. We're a global innovation partner enabling customers in communications, industrial automation, aerospace and defense, automotive, semiconductor, and general electronics markets to accelerate innovation to connect and secure the world. Learn more at Keysight Newsroom and www.keysight.com

Keysight Contact:

Paul Erwin, Americas/Europe
+1 248 430–9075
[email protected]

Fusako Dohi, Asia 
+81 42 660–2162
[email protected]