What are you looking for?
Keysight Introduces Battery Emulation and Profiling Solution for IoT Devices
- Complete emulation solution identifies the impact of variables affecting the battery drain of internet of things devices to enable design improvements
- Solution speeds and simplifies battery life testing with automation and integrated emulation and profiling capabilities
- Emulation allows engineers to achieve longer battery run time and reduce device size while shortening time-to-market
SANTA ROSA, Calif. March 21, 2023
Keysight Technologies, Inc. (NYSE: KEYS) introduces the Keysight E36731A Battery Emulator and Profiler, a complete emulation solution that identifies the impact of variables affecting the battery drain of internet of things (IoT) devices to enable development engineers to improve their device designs.
International Data Corporation (IDC) estimates that there will be 41.6 billion connected IoT devices in use by 20251, many of which will be portable, battery-operated devices requiring advanced battery management techniques. To ensure these devices perform well in the field, development engineers need to design for peak battery performance and validate those designs against real-life performance. However, testing the run time of a physical battery in a device is a challenging and time consuming task that can slow time-to-market.
The Keysight E36731A Battery Emulator and Profiler addresses the battery testing needs of IoT device designers by giving them an integrated electronic load and power supply that can be used to emulate battery performance. By testing with an emulated battery, engineers can quickly assess the effect of design or software changes on battery life by instantly transitioning the battery's charge state, allowing them to enhance their designs to achieve longer battery life and reduce device size.
The Battery Emulator and Profiler works with the Keysight PathWave BenchVue Advanced Battery Test and Emulation Software to provide a complete solution that:
- Generates Battery Profiles – By generating battery profiles, the solution allows designers to establish known, good references with consistent properties that can be used over and over to simulate battery drain. Profiles can be linked to factors such as age and temperature.
- Increases Battery Profile Accuracy – By using the simulated current drain of a device to generate battery profiles, engineers can enhance the accuracy of profiles compared to using generic manufacturer models, which leads to better device designs.
- Speeds Testing with Battery Emulation – An emulated battery allows development engineers to instantly transition a battery's charge state and gain real-time insight into current drain. This increases efficiency and allows engineers to optimize designs for longer run time.
- Automates Battery Run-Down and Cycle Testing – By automating these tests, engineers can more accurately estimate battery run time and aging effects.
- Offers Flexibility – The solution provides power up to 200W, 30V, 20A and offers a wide dynamic measurement range from microamps to amps.
Carol Leh, Vice President and General Manager for Keysight's Electronic Industrial Solutions Group's Center of Excellence, said: "The Keysight E36731A Battery Emulator and Profiler offers a valuable solution to design engineers who want to enhance their device designs. Rather than relying on intricate and time-consuming manual tests, the emulator allows engineers to quickly identify the current drain effect of critical factors such as hardware changes, software updates, and temperature changes. This way, engineers can save time and improve their device designs by using an emulated battery for testing, without the need for physical batteries."
1Worldwide Global DataSphere IoT Device and Data Forecast, 2019-2023, International Data Corporation
Resources
- Webcast: Design for Better Battery Life
- Keysight E36731A Battery Emulator and Profiler
- Data Sheet: Keysight E36731A
- Keysight PathWave BenchVue Advanced Battery Test and Emulation Software
- Keysight Low Power Battery Emulation Portfolio
- White Paper: Power the Internet of Things with End-to-End Battery Testing
- White Paper: 4 ways to Enhance Battery Performance and Insight with Emulation Software
About Keysight Technologies
At Keysight (NYSE: KEYS), we inspire and empower innovators to bring world-changing technologies to life. As an S&P 500 company, we’re delivering market-leading design, emulation, and test solutions to help engineers develop and deploy faster, with less risk, throughout the entire product lifecycle. We’re a global innovation partner enabling customers in communications, industrial automation, aerospace and defense, automotive, semiconductor, and general electronics markets to accelerate innovation to connect and secure the world. Learn more at Keysight Newsroom and www.keysight.com..
Keysight Contact:
Geri Lynne LaCombe, Americas/Europe
+1 303 662–4748
[email protected]
Fusako Dohi, Asia
+81 42 660–2162
[email protected]
The new Keysight E36731A Battery Emulator and Profiler is a complete emulation solution that allows development engineers to improve the designs of their internet of things devices.
Need to contact Media Relations at Keysight?