Keysight Introduces Pulse Generator Option for Handheld Analyzers  

  • New software application makes FieldFox the industry’s only handheld analyzer with a built-in signal generator at frequencies up to 54 GHz
  • Generates pulses including FM chirps, FM triangles, AM pulses, and custom sequences as well as continuous wave signals with a variety of analog modulations and user-defined pulse sequences
  • Highly sought-after capability supports uses including air traffic control radar testing, simulating automotive radar, and conducting radio frequency leakage checks

SANTA ROSA, Calif. May 07, 2024 

Keysight Technologies, Inc. (NYSE: KEYS) has expanded the software applications for its FieldFox portfolio of handheld radio frequency (RF) analyzers to include a pulse generator. Available for B- and C-Series FieldFox handheld analyzers, the downloadable Option 357 pulse generator offers field engineers a diverse array of pulse types at frequencies up to 54 GHz.

Field engineers conduct routine maintenance on and troubleshoot RF, microwave, and millimeter wave (mmWave) systems. During their work, they need to test a variety of devices and systems to ensure they are working as intended by using the data signals created by a pulse generator. To generate the diverse types of pulses needed for field testing, engineers need multiple expensive pulse generators that may not be specifically designed for field use.

The Keysight FieldFox Option 357 signal generator software addresses this challenge by enabling engineers to quickly upgrade existing B- and C-Series FieldFox handheld analyzers to meet their specific testing needs on the fly. All that is needed for field engineers to take advantage of the only handheld analyzer in the industry with an embedded pulse generator is a software license key and a firmware upgrade.

The new Option 357 signal generator application offers the following benefits:

  • Maximum carrier frequency coverage – Operates at frequencies up to 54 GHz depending on the FieldFox model used.
  • Wide array of pulse types – Includes standard pulses, FM chirps, FM triangles, AM pulses, and user-definable pulse sequences. In addition, it can create continuous wave (CW) signals with or without AM / FM modulations, including Frequency Shift Keying (FSK) and Binary Phase Shift Keying (BPSK).
  • Easy-to-read interface – Displays key parameters of the generated signal in both numerical and graphical formats.
  • Multiple field uses – Supports applications including field radar testing for air traffic control, simulating automotive radar, conducting field EMI leakage checks, and testing the propagation loss of mobile networks.
  • Optimize field instrument investment – Enables engineers to quickly add pulse generation capabilities to existing FieldFox handhelds to save time and money.

Vince Nguyen, Vice President and General Manager, Aerospace, Defense, and Government Solution Group at Keysight, said: “When engineers are in the field, they need flexible test solutions that can be adapted quickly to rapidly changing needs. With the FieldFox Option 357 pulse generator software application, Keysight is delivering a long sought-after capability for high-impact field applications in the aerospace, automotive, and telecommunications industries. As the only handheld analyzer that features a built-in pulse generator covering up to 54 GHz, FieldFox optimizes field instrument investments with a software-defined platform that can easily be configured through software license keys.”

Resources

 

About Keysight Technologies

At Keysight (NYSE: KEYS), we inspire and empower innovators to bring world-changing technologies to life. As an S&P 500 company, we're delivering market-leading design, emulation, and test solutions to help engineers develop and deploy faster, with less risk, throughout the entire product life cycle. We're a global innovation partner enabling customers in communications, industrial automation, aerospace and defense, automotive, semiconductor, and general electronics markets to accelerate innovation to connect and secure the world. Learn more at Keysight Newsroom and www.keysight.com.

Keysight Contact:

Paul Erwin, Americas
+1 248 430–9075
paul.erwin@keysight.com

Fusako Dohi, Asia 
+81 42 660–2162
fusako_dohi@keysight.com

Jenny Gallacher, Europe
+44 (0) 7800 737–982
jenny.gallacher@keysight.com 

Netherlands