What are you looking for?
Network Visibility Solutions
Improve your network security and monitoring insights
The directive for many IT departments is to be part of the business innovation process. How do you innovate? The average IT team spends more than half of their day just on problem resolution or network security issues.
Network visibility starts at the foundation of your network. It allows you to expose and resolve hidden problems (blind spots) faster. Faster resolution times mean more TIME to innovate the network design and the applications running on top of it.
Network Visibility Technology Partners
Best-of-breed solutions for security, performance, and the cloud.
Improve Network Visibility
Better network visibility delivers the highest performance data access and data distribution to your monitoring and security appliances.
Learn how easy it is to innovate your inline security and out-of-band network visibility.
Network Visibility for Enterprises
The new business environment demands IT support for a wider range of monitoring, security, and compliance requirements. This creates significant burdens on network performance and network security as more appliances need access to incoming data.
See how better network visibility can help you:
- Improve the security of your network
- Decrease troubleshooting costs and time
- Satisfy regulatory compliance initiatives
Network Visibility for Service Providers
Service Providers need clear visibility into their networks. Questions like these arise daily:
- Where are traffic bottlenecks?
- Why are applications running slow?
- Do I have a security problem?
These are serious questions that need quick and complete answers. See how the deployment of a visibility architecture can eliminate network blind spots to give you the answers you need.
Are you an expert on network monitoring terminology?
If not, learn what all the terms mean. Becoming an expert is easier than you think. In fact, it is as simple as the ABC's of Network Visibility.
Network Visibility Use Cases
Once you see what network visibility can do, you will discover lots of use cases where it can be applied. While not all solutions apply to every network, every enterprise should be able to find at least one.
Look at these general categories to see where visibility solutions can change business outcomes:
- Improve network security
- Provide cost reduction capabilities
- Speed up troubleshooting efforts
- Remove network blind spots
- Optimize network performance
- Strengthen regulatory compliance initiatives
Architecting For Network Visibility
When selecting a visibility architecture, performance matters.
Measure for yourself why we are the industry leader in network packet broker performance.
4X Better Performance
If you had a choice between one processor and two, which would you pick? Our network packet brokers have four times higher performance because we use a high-performance FPGA to make sure you never drop a packet.
8X Easier to Use
Would you rather program every connection one at a time or drag and drop them? What if one way was much faster and much less prone to mistakes? Find out how:
Zero Packet Loss
Would you be worried if your network packet broker was dropping packets? You should put yours to the test because many customers are discovering their current visibility solution is not keeping up.
High Availability
Will you still be protected if your security infrastructure suffers a temporary outage? Or be able to upgrade without service disruption? Make sure security and monitoring tools can recover from unexpected disruptions with the industry's fastest failover.
Concurrent Features
You buy a full-featured network packet broker because of its rich feature set. You should ensure that you can run simultaneous features since some packet brokers do not allow that. Ixia network packet brokers give you the flexibility and choice to select and deploy the features you want and need.
Network Visibility Solutions
Inline Security
Inline security products and solutions can inspect live traffic without risk to availability, ensure continuous security with fast failover, and update security appliances without downtime.
Out-of-Band Monitoring
Out-of-band monitoring products and solutions give tools access to all relevant network traffic, deliver data with speed and accuracy, and make changes easily, as often as you need
Security Needs To Be In The Fabric Of Your Network
The Ixia Security Fabric uses context-awareness and security intelligence to deliver de-duplicated and highly relevant traffic to your inline and out-of-band security and monitoring tools. Powered by dual data processing engines, Security Fabric is the foundation for more robust inline security and faster out-of-band compliance and monitoring.
Make sure you have complete data access, resilience, context-aware data processing, and security intelligence processing to ensure the right data gets to the right tools, even at high speeds.
Further Reading
CATALOGS - start planning today
Network Visibility
Build a visibility fabric - network packet brokers, taps, bypass switches and more.
Network Performance and Security
Know how your network is running so you can hit tough SLAs - then secure it.
Let us help you build a highly resilient, total visibility architecture to maximize your security and optimize performance.