INTELLIGENT VISIBILITY

Visibility powered by a multi-layer security fabric improves enterprise network monitoring performance.

Intelligent network visibility allows IT to strengthen network security, reduce monitoring costs, increase return on investment (ROI), and optimize network performance. Keysight offers the widest range of network taps, virtual network taps, and intelligent network packet brokers (NPBs) that allow you to:

visibility benefits
Remove Blind Spots and Improve Network Monitoring

REMOVE BLIND SPOTS AND IMPROVE NETWORK MONITORING

Blind spots occur when data is lost on its way to the monitoring and compliance tools or also when security incident data has become buried. Blind spots can occur because of overloaded SPAN ports, not using a Network Packet Broker (NPB) properly sized for your network, or lack of connectivity for tools like DLPs, SIEMs, logging tools, protocol analyzers, etc. It is very common for these blind spots to contribute to network outages, performance issues, security breaches, and compliance problems. The easiest and best answer to solving the problem is to implement a scalable visibility architecture with the industry’s most reliable Taps and highest performing NPBs.

Learn more about how Keysight Network Taps and NPB solutions eliminate blind spots in your network.

CONTEXT AWARENESS SUPERCHARGES NETWORK MONITORING PERFORMANCE

Context awareness is a powerful capability to improve network operations. Context-aware data processing allows the right data to be distributed the right tools through data deduplication, packet trimming, burst protection, and especially application level filtering. These combined features help expose indicators of compromise, identify geolocation of users and devices, and improve troubleshooting efforts.

EXTEND THE LIFE OF EXISTING MONITORING TOOL INVESTMENTS

Modern enterprise networks typically have several problems when it comes to getting the most value out of their monitoring tools. A visibility solution provides capabilities for clear cost reductions by eliminating various issues like:

  • Access to the proper data
  • Reducing the need to constantly add new monitoring tools
  • Ensuring monitoring tool capabilities match the network security

An intelligent visibility framework helps every monitoring tool see more and focus in on the data that matters most to you.

Learn more about how Keysight can help you extend the life of your monitoring tools:

Extend the life of existing monitoring tool investments
maximize network performance to see the whole picture

MAXIMIZE NETWORK PERFORMANCE TO SEE THE WHOLE PICTURE

IT security and analytics tools are only as good as the data they are seeing. Performance matters — don't settle for partial visibility due to dropped packets within your solution. Your tools need complete visibility to properly monitor the network.

In addition, proactive monitoring lets you perform real testing of your network to validate network/application performance and measure SLAs whenever you need to.

Learn more about how Keysight can help you see what you have been missing and maximize network performance:

Visibility Enhances Regulatory Compliance

Better network visibility and control of data allows enterprises to enhance regulatory compliance. This includes PCI DSS, HIPAA, lawful intercept, and various other compliance initiatives. The key is to capture the proper data, segment it out, and then deliver it to the proper location.

Learn more about how Keysight can help you enhance regulatory compliance:

White Papers 2022.01.07

Visibility Architecture – Eliminating Visibility and Security Blind Spots

Visibility Architecture – Eliminating Visibility and Security Blind Spots

2022.01.07

Visibility Architecture – Eliminating Visibility and Security Blind Spots

According to ZK Research, 85% of the mean time to repair (MTTR) is the time taken to identify there is in fact, an issue. If your IT department cannot quickly identify problems, chances are they will constantly hear about issues from unhappy customers. And once the MTTR clock starts ticking, there’s no telling whether IT knows there is an issue or not. If you’re trying to ensure your networks are fast, reliable and secure through approaches that attempt to manage each aspect of their performance—from Network Ops, Application Ops, Security Admins, Server Admins, Forensics, and Privacy and Audit teams—chances are that each of these teams purchased their own set of analytics or monitoring tools. For many, these solutions have not solved the problem, leaving unidentified blind spots that remain a looming threat. In this insightful white paper, Visibility Architecture: Eliminating Visibility and Security Blind Spots, you’ll learn about a once-in-a-generation change that’s creating a shift to public and private cloud computing, virtualized networking, and the growing number of connected devices are structurally changing IT. What you will learn: First, what are the components of good visibility and security? Second, how a visibility architecture can give you 100% ROI, with vastly improved problem identification, isolation, and repair times. Third, how you can effectively comport with many compliance mandates. Fourth, achieve end-to-end visibility for both physical and virtual networks. Fifth, don’t wait for disjointed approaches to security and visibility to create an unforeseen problem. Read this white paper to get the insights you need to make better decisions.

Reduce Your Network Downtime And Mean Time To Repair

During breaches and outages, minutes matter. This is where a visibility architecture can reduce network downtime. Once a tap and network packet broker (NPB) are inserted into the network you can drastically reduce Change Board approvals and the use of Crash Carts for troubleshooting. Your processes and capabilities will be faster than before, especially when remote access capability is deployed.

Learn more about how Keysight delivers the solution you need to reduce downtime:

Reduce MTTR
Tap Into Your Data Where and When You Need It

Tap Into Your Data Where And When You Need It

Network visibility starts with capturing the proper data from physical and virtual networks (both public and private) to enable a deeper, richer understanding of your network.

The data you may need can come from anywhere within your network. Deploy the physical and virtual taps you need, where you need to get that data. This gives your monitoring solution the right data so it can be delivered to the right tool when needed.

Keysight is the number one vendor in the network taps market. Learn more how Keysight can help you tap your network:

Maximize the value of security and monitoring tools.

Find out more.

Switzerland