Highlights

  • Tablet-based user interface: The tablet's interface is designed for touchscreen use, making the solution discreet and user-friendly.
  • Professional in-building features: These include automated augmented reality-based indoor positioning, indoor maps with geodetic coordinates, and instant reports, which make indoor testing efficient.
  • Lightweight and portable: The backpack's lightweight design supports 12 test devices and a portable scanner, allowing for extended, comfortable use throughout the day. Four hot-swap batteries, and quick charging solutions enable up to 24 hours of uninterrupted measurements.
  • Reliable: The cable-connected system ensures a reliable connection for the tablet and test devices, and two cooling fans maintain the temperature control and keep the phones connected to 5G NR even during heavy tests.
  • High-end design with free over-the-air (OTA) reception: The carbon fiber design provides free over-the-air RF reception to all measurement phones, enabling scientific quality of experience (QoE) measurements without RF blockage.
  • Versatile: The same solution can be used for indoor walk testing and in-car drive testing.
  • Future-proof: Keysight Nemo products have a track record of being the first to support new technologies and the latest smartphones.
Man carrying a backpack and tablet in office

Ensure Mobile Network Quality in Indoor Environments

As mobile network traffic increasingly shifts indoors, operators face the challenge of ensuring uninterrupted connectivity in environments such as malls, arenas, campuses, and stations. Traditional drive testing methods are often impractical in these settings, requiring specialized indoor benchmarking solutions.

Mobile network operators and network regulators can leverage the Nemo Backpack Air Pro to perform all necessary measurements for indoor benchmarking in a single run, reducing the time and costs associated with measurement campaigns. The solution ensures that operators can maintain high-quality service for customers in indoor locations, where the majority of mobile network traffic occurs.

Nemo Backpack Air Pro provides a reliable, cable-connected system that supports up to 12 devices, enabling operators to perform comprehensive benchmarking in one go. The versatile Nemo Backpack Air Pro is also ideal for in-building testing and in-car drive testing.

Support for a Wide Selection of Android-Based Devices

Nemo Backpack Air Pro enables extensive synchronized measurements and scripted events across up to 12 terminals. A single tablet acts as the controller unit, orchestrating multi-measurements by sending commands to agent units. Log files can be seamlessly uploaded to Nemo Cloud or FTP/HTTP servers, and the collected data can be directly analyzed using Nemo Analyze.

Nemo Backpack Air Pro, together with the Nemo Diagnostic Module (NDM), enables full measurement functionality with commercial off-the-shelf smartphones, without the need for special firmware or rooting. This product supports the latest smartphones and tablets, including the Samsung Galaxy Tab S10+, all models in the Samsung Galaxy S24, S23, and S22 family, Sony Xperia 1 VI models, and the Motorola Edge 40 Ultra.

Two people looking at computer screen with Nemo Cloud software

Want help or have questions?

France