Choose a country or area to see content specific to your location
Bestätigen Sie Ihr Land oder Gebiet
Deutschland Deutschland
Bitte bestätigen
Confirm your country to access relevant pricing, special offers, events, and contact information.
Simplify wideband characterization. Save up to 15% on aerospace and defense component testing.
Enable faster, flexible testing for 802.3ck and PCIe® 6.0 designs with a 50+ GHz probe.
Get your choice of two free software applications with the purchase of an HD3 Oscilloscope.
Enable accurate real-time analysis for wireless, and radar with up to 4 GHz bandwidth signal analyzers.
Gain greater measurement insight at low current resolution.
Discover the precision, performance, and compact designs of our signal sources and analyzers.
ADS streamlines design verification and compliance through standards-driven workflows.
State-of-the-art ray tracing solution for quick, accurate site-specific RF propagation scenario creation.
Achieve 200+ Gbaud multi-level modulated signals with high-speed AWGs for digital and optical standards.
Comply with 2025 CMMC mandates and advance your IT cybersecurity with Keysight. Download our white paper.
With extra memory and storage, NPBs run Keysight's AI security and performance software and AI stack.
Explore curated support plans, prioritized to keep you innovating at speed.
Explore engineer-authored content and a vast knowledge base with thousands of learning opportunities.
Keysight Learn offers immersive content on topics of interest, including solutions, blogs, events, and more.
Quick access to the most frequent support related self-help tasks.
Additional content to support your product needs.
Explore services to accelerate every step of your innovation journey.
Use an oscilloscope to make 11 essential switch mode power supply measurements that will help you characterize and optimize your SMPS.
Learn:
Lesson 1 - SMPS Measurement Basics
Introduces the basics of switch-mode power supply (SMPS) testing and the key measurements that can be used to characterize an SMPS. The lesson also covers the different types of oscilloscopes that can be used for SMPS testing and the different types of probes that can be used.
Lesson 2 - AC Input/Power Quality
Covers the quality of the AC input power to a switch-mode power supply (SMPS). It covers topics such as the different types of power quality disturbances, how to measure them, and how they can affect the performance of an SMPS.
Lesson 3 - Current Harmonics
Discusses the harmonic content of the current drawn by an SMPS. It covers topics such as the different types of harmonics, how to measure them, and how they can affect the power grid.
Lesson 4 - Inrush Current
Explains the inrush current of an SMPS. Inrush current is the surge of current that occurs when an SMPS is first turned on. It is caused by the capacitors in the SMPS charging up. Inrush current can be a problem because it can overload the AC input power source and cause voltage sags.
Lesson 5 - Modulation Analysis
Covers the modulation techniques used in SMPS. Modulation is the process of changing the amplitude, frequency, or phase of a signal. In SMPS, modulation is used to control the output voltage of the power supply.
Lesson 6 - Rds(on) and Vce(sat)
Discusses the on-resistance (Rds(on)) and saturation voltage (Vce(sat)) of power MOSFETs. These are two important parameters that determine the efficiency and performance of an SMPS.
Lesson 7 - Slew Rate
Focuses on the slew rate of a power MOSFET. The slew rate is a measure of how quickly the voltage across a MOSFET can change. It is an important parameter that determines the dynamic performance of an SMPS.
Lesson 8 - Output Ripple
Explains the output ripple of a switch-mode power supply (SMPS). It covers topics such as the different types of output ripple, how to measure them, and how they can affect the performance of an SMPS.
Lesson 9 - Turn on and Turn off Time
Discusses the turn on and turn off times of a switch-mode power supply (SMPS). It covers topics such as the different factors that affect these times, how to measure them, and how they can affect the performance of an SMPS.
Lesson 10 - Transient Response
Discusses the transient response of a switch-mode power supply (SMPS). It covers topics such as the different types of transients, how to measure them, and how they can affect the performance of an SMPS.
Lesson 11 - Efficiency
Discusses the efficiency of an SMPS. It covers topics such as the different factors that affect efficiency, how to measure efficiency, and how to improve efficiency.
Bench and Power Products
As devices have changed, so have your testing needs. Today’s designs are increasingly portable and connected. Troubleshooting DC to radio-frequency (RF) technologies requires a variety of instruments, and Keysight offers the deepest bench in the industry.
eBooks
Switch Mode Power Supply Analysis
From laptops to vacuum cleaners, all electrical products have one thing in common: a power supply. Without stable, well-regulated DC power, devices can malfunction. If you do not test for this properly during the design phase, it could damage other components in your design or, worse, delay your entire project.
Applikationsberichte
How to Make the Best Switch Mode Power Supply Measurements
Characterizing the operation of switch mode power supplies requires a broad range of measurements. Most of the required measurements can be performed using an oscilloscope. However, many engineers today still perform these measurements manually on their scopes, which is very time consuming.
How to Test Switch Mode Power Supplies
Automate input, switching, output and frequency response measurements
Können wir Ihnen behilflich sein?