NCAP scenarios testing must cover several test cases for common radar-based advanced driver assistance systems (ADAS) and autonomous vehicle (AV) features and functions. To reproduce the scenes precisely, automotive manufacturers require a solution to render full 3D scenes in the lab with the goal of testing the real sensor response. Forward collision warning and autonomous emergency braking systems use cameras, lidar, or radar sensors individually or in concert (sensor fusion). However, each sensor offers a varying degree of performance.
Emulating real-world driving scenarios in the lab requires a full-scene emulator that can be used to test the radar sensors with varying driving speed, direction, distance, and number of targets across a contiguous field of view (FOV). Radar sensors must also be tested against variable environmental conditions, such as RF-dense urban scenes with interference, and surrounding landscape, to ensure confidence in their performance.
Autonomous driving NCAP scenarios test solution
Emulating complex traffic scenes requires a full-scene emulator that bridges the gap between software simulation and on-road testing. Keysight Radar Scene Emulator enables you to emulate real-world driving scenarios — various speeds, distances, and number of targets — across a contiguous field of view. Achieve your vision of an advanced driver assistance system (ADAS) and next-generation vehicle autonomy sooner and with less risk, using radar sensors and software that you can test against the complexity of real-world driving scenarios.
See demo of autonomous driving NCAP scenarios testing
Video Player is loading.
Current Time 0:00
/
Duration -:-
Loaded: 0%
Stream Type LIVE
Remaining Time -0:00
1x
2x
1.5x
1x, selected
0.5x
Chapters
descriptions off, selected
subtitles off, selected
This is a modal window.
The media could not be loaded, either because the server or network failed or because the format is not supported.
Creating safe and robust autonomous driving (AD) systems is complex. Autonomous vehicles (AVs) have hundreds of sensors needing to work with one another inside the car and with other smart vehicles. The software algorithms enabling AD features will ultimately need to synthesize all the information collected from these sensors to ensure the vehicle responds appropriately. These algorithms require testing against millions of complex scenes covering various driving scenarios. Explore the Keysight radar scene emulator's three main differentiators – extended object emulation, minimum distance, and wide FOV with many objects. This modal can be closed by pressing the Escape key or activating the close button.
Explore products in our autonomous driving NCAP scenarios test solution