Choose a country or area to see content specific to your location
Verifying Wi-Fi® devices on the manufacturing line requires a multi-port test chassis with high port density to support the multi-antenna and multi-radio designs of the latest Wi-Fi standards. The test set must be capable of running non-signaling tests on multiple devices-under-test at once. High-volume, high-speed testing is achieved by scheduling test execution across multiple test sets concurrently. Test sets must support all Wi-Fi frequencies including 2.4 GHz, 5 GHz, 6 GHz, and 7.3 GHz, with bandwidth up to 800 MHz. Support for other standards including 5G, Bluetooth®, and near-field communications (NFC) is desirable if the device supports multiple radio standards.
Design verification and manufacturing tests for transmitters include transmit spectral mask, spectral flatness, and modulation accuracy. Test solutions that can generate baseband signals will be able to verify the RF requirements for receivers, including receiver minimum input sensitivity, adjacent and non-adjacent channel rejection, and receiver maximum input level. For design verification and manufacturing test, the test solution must be capable to calibrate and verify multiple client devices, multiple access points, multiple antennas with different frequency ranges, and verify RF performance with MIMO.
Design verification and manufacturing test for Wi-Fi devices requires non-signaling tests for the latest Wi-Fi standards, including 802.11be, plus support for other radios in the device-under-test, such as 5G NR FR1, and Bluetooth® 5.1. The Keysight Wi-Fi test and validation solution consists of the Keysight wireless test set and Keysight X-Series measurement software. The solution dynamically configures port assignments based on the wireless standard being tested, and can test multiple devices in parallel. Tests are sequenced and automated using internal switching between ports. Test throughput can be scaled during design verification and manufacturing with test set control, automation, and sequencing software.
How to Perform Wi-Fi® Device Manufacturing Tests
Keysight's E6680A is the solution to test WLAN devices today and tomorrow. Ready for the future with up to 800 MHz bandwidth, it analyzes the 320 MHz signals defined for IEEE 802.11be.
Number of Transceivers |
|
Number of Ports Per Transceiver | 8 |
Frequency Range |
|
Bandwidth Options |
|
Technology |
|
How to Perform Wi-Fi® Device Manufacturing Tests
One-button measurements for WLAN 802.11a/b/g/j/p/n/af/ah transmitters
Activity |
|
Hardware Connectivity |
|
Technology |
|
License Types |
|
Software Type |
|
Industry Segment |
|
How to Perform Wi-Fi® Device Manufacturing Tests
One-button measurements for WLAN 802.11ac/ax transmitters
Activity |
|
Hardware Connectivity |
|
Technology |
|
License Types |
|
Software Type |
|
Industry Segment |
|
How to Perform Wi-Fi® Device Manufacturing Tests
Perform WLAN 802.11be one-button measurements defined by IEEE 802.11 standard
License Types |
|
Software Type |
|
Industry Segment |
|
Technology |
|
Additional resources for Wi-Fi device manufacturing testing
Simulating a 5G NTN RF link and channel model for a transmit/receive pair between the gateway, the satellite, and the user equipment in a transparent payload architecture requires a platform compliant with 3GPP Release 17. Learn how to meet these requirements using the Keysight System Design simulation software.
Learn More
Measuring 5G private network base station transmitter signal quality requires a high-frequency and wide-bandwidth test system that can address excessive path loss, wideband noise, and frequency errors with minimum impact on the EVM test results. Learn how to measure accurate signal quality in your 5G private network base station transmitters for your 5G new radio (NR) frequency range 1 (FR1) and FR2 applications.
Learn More
NTN test requires laboratory reconstruction of all possible NTN scenario permutations. Learn how to perform end-to-end testing and validation of NTN deployments.
Learn More
Need help finding the right solution for you?
Bluetooth® and the Bluetooth® logos are registered trademarks owned by Bluetooth SIG, Inc., and any use of such marks by Keysight Technologies is under license.