Highlights

Communicate, Measure, Organize

Labber offers a complete, easy-to-use solution for instrument control and lab automation. The software is suitable for any R&D, test, or measurement team that wishes to bring its experimental potential to its maximum. Successful researchers and engineers should not have to invest time writing many lines of code before running an experiment. Instead, they should spend their time running tests and measurements.

INSTRUMENT SERVER

The instrument server handles communication with all the instruments and equipment present in the experimental laboratory setup.

Labber supports communication over GPIB, serial, USB, TCP / IP, and any other interface that is implemented by the VISA standard.

See our GitHub repository for a complete list of available instrument drivers. On top of the instrument drivers, there is also a set of virtual drivers that are used to implement additional functionality needed for different experiments.

RUN MEASUREMENTS

The measurement setup dialog defines the sequence of values to set or measure during an experiment.

Sequences can have an arbitrary number of dimensions. You can easily create them using drag-and-drop functionality.

Add comments, tags, and users for easy tracking of experiments among your team and efficient collaboration.

LOG BROWSER

The log browser visualizes the contents of the log database. In addition to the date of measurement, you can organize your log files using tags such as project name, chip number, or user.

The log list shows a list of logs matching the selected tags. Quick view shows data and settings for the currently selected log.

Logs can be starred to highlight important data. Double-clicking an individual log brings up the log viewer.

Want help or have questions?

Vietnam