Keysight Makes UK’s First 100Gbps 6G Sub-THz Connection with National Physical Laboratory and University of Surrey

  • Data link made at speeds greater than 100 Gbps at a frequency of 300 GHz using both 32 and 64 quadrature amplitude modulation
  • Achievement enabled by Keysight's 6G sub-THz testbed platform

SANTA ROSA, Calif. April 24, 2023 

Keysight Technologies, Inc. (NYSE: KEYS), in collaboration with National Physical Laboratory (NPL) and the University of Surrey, has made the first 6G connection at speeds greater than 100 gigabits per second (Gbps) over sub-terahertz (THz) frequencies in the U.K.  

Future 6G use cases, such as augmented reality and autonomous vehicles, will require data throughput speeds from 100 Gbps to 1 terabit per second (Tbps). To achieve the extreme data speeds and low latencies required by these revolutionary use cases, the use of sub-THz frequencies is being explored. However, operations in sub-THz frequency bands introduce signal integrity and path loss challenges that can negatively impact performance.

Keysight, NPL, and the University of Surrey established the first sub-THz high throughput 6G testbed in the U.K. to address these challenges. Funded by the U.K. government for 6G research, NPL and Surrey scientists are using the testbed to study and characterize sub-THz signal performance to generate new techniques for optimizing data paths and calibration methodologies.

Located at NPL, this new 6G testbed achieved the U.K.'s first high-speed sub-THz data link. The demonstration was made at a frequency of 300 GHz using both 32 and 64 quadrature amplitude modulation (QAM). Built on Keysight's 6G Sub-Terahertz R&D Testbed, the testbed uses the M8194A Arbitrary Waveform Generator (AWG) combined with Virginia Diodes Inc. (VDI) upconverters / downconverters to generate the signal and Keysight's UXR0704A Infiniium multichannel high-performance 70 GHz oscilloscope to analyze the signal.

Keysight, NPL, and the University of Surrey will demonstrate the new 6G testbed at the Spring 2023 6G Symposium at the University of Surrey, April 24-26.

Irshaad Fatadin, Principal Scientist, National Physical Laboratory, said: "6G is a key focus for NPL and we are using our scientific and measurement capabilities to tackle the challenges of this new technology. Our partnership with Keysight will be a critical success factor in our 6G research work."

Mosaab Abughalib, Senior Research Director and General Manager for Keysight's Network Emulation Group, said: "Through this partnership we are bringing Keysight solutions and experts together with scientists from NPL and the University of Surrey to unlock the true potential of 6G."

Resources

About Keysight in 6G
Keysight creates the runway that enables researchers to launch evolutionary and revolutionary technology platform solutions based on 5G-Advanced and 6G technologies. A cohesive set of design and development building blocks across multiple interconnected technology domains enables innovators to spark new insights. Keysight plays a pivotal role in bringing to life 6G use cases that have the potential to transform society, enhance human interactions, enable enterprises to achieve greater efficiencies, and accelerate life-changing innovations.

About Keysight Technologies

At Keysight (NYSE: KEYS), we inspire and empower innovators to bring world-changing technologies to life. As an S&P 500 company, we’re delivering market-leading design, emulation, and test solutions to help engineers develop and deploy faster, with less risk, throughout the entire product lifecycle. We’re a global innovation partner enabling customers in communications, industrial automation, aerospace and defense, automotive, semiconductor, and general electronics markets to accelerate innovation to connect and secure the world. Learn more at Keysight Newsroom and www.keysight.com..

Keysight Contact:

Geri Lynne LaCombe, Americas/Europe
+1 303 662–4748
[email protected]

Fusako Dohi, Asia
+81 42 660–2162
[email protected]