Lesson 3 - What is a Signal Generator?
Review the basic concepts of signal generators and their applications. The lesson begins by defining what a signal generator is and how it works. It then discusses the different types of signal generators, including arbitrary waveform generators, function generators, and pulse generators. The lesson also covers the key parameters that are used to characterize signal generators, such as frequency range, amplitude range, and output power.