Keysight Introduces Comprehensive LPDDR6 Solution for End-to-End Memory Design and Test Workflows

  • Delivers complete design and validation solution for Low-Power Double Data Rate 6 (LPDDR6) memory in mobile, client computing, and AI applications.
  • Supports JEDEC’s ongoing development of the new LPDDR6 memory standard.
  • Enables enhanced performance analysis focusing on speed optimization, power efficiency, and reliability testing.
  • Features advanced measurement-based noise compensation technology for superior signal integrity.

SANTA ROSA, Calif. January 27, 2025

Keysight Technologies, Inc. (NYSE: KEYS) announced the Low-Power Double Data Rate 6 (LPDDR6) design and test solution, a complete design and test solution to support the next technology wave for memory systems. The solution significantly improves device and system validation, providing new test automation tools necessary for advancing AI, especially in mobile and edge devices.

The memory market is evolving due to the rising demand for high-performance computing, AI, and energy-efficient mobile applications. LPDDR6 significantly enhances performance and efficiency to support next-generation compute system requirements, making it a crucial upgrade for contemporary devices.

Test complexity has grown with the adoption of next-generation memory devices such as LPDDR6, HBM4, and GDDR7. These technologies demand advanced test methods to ensure reliability and performance, and reducing test times while maintaining accuracy is a constant challenge.

Keysight’s complete workflow solution consists of transmitter and receiver test applications and the Advanced Design System (ADS) Memory Designer workflow solution. The LPDDR6 test solution can be paired with Keysight EDA software and the Keysight Memory Designer bundle to achieve faster design confidence from simulation to verification and test. The LPDDR6 test automation solution is based on Keysight’s UXR oscilloscope and high-performance M8040A Bit Error Ratio Tester.

LPDDR6’s impact is expected to reach beyond mobile devices. The new memory standard’s combination of high performance and power efficiency makes it particularly suitable for AI and machine learning applications, high-speed digital computing, automotive systems, data centers, and other edge applications areas where the balance between processing power and energy consumption is crucial.

Key Benefits of Keysight’s LPDDR6 Test Solution:

Accelerate Time-to-Market with Advanced Transmitter Testing

  • Reduce validation time with fully automated compliance testing and characterization
  • Capture precise measurements quickly using industry-leading low-noise technology
  • Debug design issues faster with streamlined data analysis tools
  • Analyze device BER performance with extrapolated eye mask margin testing
  • Achieve accurate signal measurements directly from BGA packages with specialized de-embedding capabilities

Optimize Device Performance with Comprehensive Receiver Testing

  • Validate designs confidently using proven Bit Error Ratio testing methodology
  • Pinpoint performance issues early by testing against multiple jitter, crosstalk, and noise scenarios
  • Maximize signal integrity through detailed BER analysis and receiver equalization optimization
  • Ensure high interoperability with both device and host controller validation

Deliver Next-Generation Memory Solutions

  • Enable faster user experiences with higher data rates support 
  • Extend battery life and reduce power consumption in mobile and data center applications
  • Build more reliable products with enhanced data integrity and system stability features

Dr. Joachim Peerlings, Vice President and General Manager, Network and Datacenter Solutions, Keysight, said: “As a leader in memory design and test solutions, Keysight continues to collaborate with JEDEC to develop the LPDDR6 standard. This new LPDDR6 standard is set to revolutionize the market, offering unprecedented speed, efficiency, and reliability, enabling the industry's AI Edge rollout. As the deployment and use of next-generation memory devices are growing, Keysight has achieved a significant milestone in enabling faster time to market for LPDDR6 memory designs.”

The new receiver and transmitter solution will be shown to the public for the first time at DesignCon 2025, Jan 29-30, at booth number 1039 in Santa Clara, California.

Resources

About Keysight Technologies   

At Keysight (NYSE: KEYS), we inspire and empower innovators to bring world-changing technologies to life. As an S&P 500 company, we're delivering market-leading design, emulation, and test solutions to help engineers develop and deploy faster, with less risk, throughout the entire product life cycle. We're a global innovation partner enabling customers in communications, industrial automation, aerospace and defense, automotive, semiconductor, and general electronics markets to accelerate innovation to connect and secure the world. Learn more at Keysight Newsroom and www.keysight.com

Contacts 

North America PR Team
pdl-americas-keysight@keysight.com

Fusako Dohi, Asia
+81 42 660–2162
fusako_dohi@keysight.com

Jenny Gallacher, Europe
+44 118 927 4003
jenny.gallacher@keysight.com

Thailand