무엇을 찾고 있습니까?
Keysight, IPG Automotive and Nordsys Collaborate to Accelerate Validation of Advanced Driver Systems
Will jointly deliver new modular test platform - Autonomous Drive Emulation (ADE) Platform
SANTA ROSA, Calif.; KARLSRUHE, Baden-Württemberg; BRAUNSCHWEIG, Lower Saxony, July 27, 2020
Keysight Technologies, Inc. (NYSE: KEYS), a leading technology company that helps enterprises, service providers and governments accelerate innovation to connect and secure the world, IPG Automotive , a global leader in virtual test driving technology and Nordsys, one of the leading companies for the development of software system architectures for vehicle-to-everything (V2X) communication, are collaborating to design and develop a modular test platform that will accelerate the validation of advanced driver-assistance systems (ADAS) and functions for autonomous driving.
The automotive industry is facing tremendous change and multiple technology disruptions. The number of sensors and quantity of data that needs to be processed by the decision-making units in ADAS-enabled cars is driving increased complexity in development, simulation and testing. In addition to the complexity associated with the technical limitations of various sensor emulation implementations, is the integration into a complete and comprehensive environment due to the lack of standard interfaces.
Keysight, IPG Automotive and Nordsys have established a multi-year collaboration to create a solution – the Autonomous Drive Emulation (ADE) platform - which will emulate synchronized connections to all relevant sensors in a car such as the global navigation satellite system (GNSS), vehicle to everything (V2X) camera and radar, in a single system.
ADE enables automotive OEMs, and their partners, to focus on the development and testing of ADAS systems and algorithms, including sensor fusion and decision-making algorithms. It is an open platform that simplifies integration with commercial 3D modeling, HIL systems and existing test and simulation environments.
"Combining the experience and expertise of Keysight, IPG and Nordsys will deliver a solution that enables customers to simulate and emulate their components, software and systems including sensor fusion and decision-making algorithms," noted vice president and general manager of Keysight's automotive industry segment, Tom Goetzl.
"Our innovative software solutions allow for transfer of real test scenarios including the entire environment into the virtual world with a high level of detail. We are delighted to bring this powerful and real-time capable software modeling technology to ADE and participate with Keysight in this partnership," commented Steffen Schmidt, managing director of IPG Automotive.
"Nordsys creates software-controlled applications focused on the automotive industry, as well as hardware and software solutions for V2X communications. We look forward to bringing this expertise to ADE and the collaboration with Keysight," said Manfred Miller, CEO of Nordsys.
About Nordsys
NORDSYS GmbH, based in Braunschweig – Germany, has over 15 years of experience in communication technology for the automotive industry and is one of the leading companies for the development of software system architectures for V2X communication. With the brand waveBEE® Nordsys offers a complete eco system for development, simulation and testing of V2X environments. As partner of prestigious vehicle manufacturers, tier-1 suppliers and technology providers the company has its key competences in driver assistant systems, infotainment, future mobility solutions and complex simulation environments.
About IPG Automotive
As a global leader in virtual test-driving technology, IPG Automotive develops innovative simulation solutions for vehicle development. The company's software and hardware products for the application areas of ADAS & automated driving, powertrain and vehicle dynamics are designed for seamless use throughout the entire development process.
About Keysight Technologies
Keysight Technologies, Inc. (NYSE: KEYS) is a leading technology company that helps enterprises, service providers and governments accelerate innovation to connect and secure the world. Keysight's solutions optimize networks and bring electronic products to market faster and at a lower cost with offerings from design simulation, to prototype validation, to manufacturing test, to optimization in networks and cloud environments. Customers span the worldwide communications ecosystem, aerospace and defense, automotive, energy, semiconductor and general electronics end markets. Keysight generated revenues of $4.3B in fiscal year 2019. More information is available at www.keysight.com.
# # #
Additional information about Keysight Technologies is available in the newsroom at https://www.keysight.com/go/news and on Facebook, LinkedIn, Twitter, and YouTube.
Nordsys Media Contact:
Maik Schlote, PR Manager
+49 531 296988-50
[email protected]
IPG Automotive Contact:
Katja Rische
+49 (721) 98520-209
[email protected]
Keysight Contact:
Geri Lynne LaCombe, Americas/Europe
+1 303 662–4748
[email protected]
Fusako Dohi, Asia
+81 42 660–2162
[email protected]
Need to contact Media Relations at Keysight?