What are you looking for?
Keysight Secures First Release 16 Power Saving Test Case Validations
- Test cases include device certification tests for radio frequency demodulation and radio resource management for frequency band n78
- First test tool validation for radio frequency performance four-component carrier aggregation downlink test cases also secured
- Keysight extends leadership with coverage of 98% of all 5G NR validated test cases
SANTA ROSA, Calif. July 31, 2023
Keysight Technologies, Inc. (NYSE: KEYS) gained approval for the industry's first 5G New Radio (NR) Release 16 (Rel-16) power saving test cases for demodulation and radio resource management (RRM) in the n78 frequency band. The validated test cases, which are for use with Keysight's 5G network emulation conformance test platform (TP168), were obtained at the recent Conformance Agreement Group (CAG) #75 meeting of the Global Certification Forum (GCF).
Optimizing power consumption is a key focus for 5G NR, with targeted improvements including extended battery life for device users. 3GPP Rel-16 addresses this need with new features that help reduce power consumption, such as RRM monitoring relaxations for devices not at a cell edge or with low mobility. Keysight's approved test cases enable certification test for devices with these features to ensure they successfully pass the conformance criteria.
Keysight also received approval at CAG #75 for the first test tool validation covering radio frequency (RF) performance four-component carrier (4CC) aggregation downlink test cases. Enabling 4CC aggregation will boost wireless throughput rates for faster downloads and better performance.
With the addition of these test cases available through the S8705A RF/RRM DVT and Conformance Toolset, Keysight extends its test case leadership by having the greatest number of new test case / band validations and activating the greatest number of new work items now available for certification testing. Currently, Keysight leads the industry with coverage of 98% of all 5G NR-validated test cases.
Muthu Kumaran, General Manager of Keysight's Device Acceptance Solutions, said: "Power Saving is a priority for the 5G NR industry and Keysight is committed to supporting the rollout of these features. In addition to securing the Release 16 demodulation and RRM validated test cases, we are working on the new power-saving test cases for Release 17. These new validated test cases firmly cement Keysight's leadership of having the best 5G NR test case coverage in the industry at 98%."
Resources
About Keysight Technologies
At Keysight (NYSE: KEYS), we inspire and empower innovators to bring world-changing technologies to life. As an S&P 500 company, we're delivering market-leading design, emulation, and test solutions to help engineers develop and deploy faster, with less risk, throughout the entire product lifecycle. We're a global innovation partner enabling customers in communications, industrial automation, aerospace and defense, automotive, semiconductor, and general electronics markets to accelerate innovation to connect and secure the world. Learn more at Keysight Newsroom and www.keysight.com.
Keysight Contact:
Paul Erwin, Americas/Europe
+1 248 430–9075
[email protected]
Fusako Dohi, Asia
+81 42 660–2162
[email protected]
Need to contact Media Relations at Keysight?