Definition of software-defined vehicle

A software-defined vehicle (SDV) is a vehicle whose operation focuses on software over hardware. SDVs prioritize software to enable vehicle functionality, unlike traditional cars built around a mechanical framework.

Software-defined vehicles are transforming how the automotive industry approaches vehicle design, development, manufacturing, and support. One similar technological shift that exemplifies this difference is cell phones. Feature phones are like traditional vehicles, offering limited functionality and features. SDVs are like smartphones, constantly evolving and remaining adaptable through ongoing software updates. This software-driven transformation is seen as a significant evolution in the automotive industry — paving the way for further technological advancements like autonomous vehicles (AV).

Benefits and challenges of software-defined vehicles

Software-defined vehicles stand poised to make a significant transformation within the automotive industry, and the technologies empowering this advancement offer both exciting benefits and substantial challenges. While SDVs represent a leap forward in the industry, overcoming these challenges is crucial to ensure a safe, secure, and trusted future for this technology.

Benefits of software-defined vehicles

  • Enhanced performance and efficiency: Software can constantly monitor engine parameters, improve fuel or battery pack efficiency, and optimize driving dynamics.
  • Improved safety: ADAS powered by sophisticated software can react faster in critical situations, leading to safer roads.
  • Evolving capabilities: New vehicle features and functionalities can be downloaded and installed over-the-air (OTA), keeping the car up to date through software updates.
  • Personalized experience: Software can tailor the driving experience to individual preferences, including customized dashboards, ambient lighting, and in-car infotainment for the driver or passengers.
  • Predictive maintenance: Software can monitor vehicle health and predict potential issues before they become major problems, saving the vehicle owner time and money.

Challenges of software-defined vehicles

  • Software complexity: The sheer quantity of code needed to manage an SDV is immense, increasing the risk of bugs and vulnerabilities.
  • Cybersecurity threats: Since software is central to SDV functionality robust cybersecurity measures are essential to protect vehicles from cyber-attacks.
  • Data privacy concerns: The vast amount of data collected by SDVs raises data privacy concerns. Clear regulations and strong data security practices are needed to ensure user trust.
  • Modular hardware and software: Current vehicle hardware is tightly coupled to the software it enables. A modular approach allows software applications to function more independently.
  • Technical expertise gap: The automotive industry will need to attract and develop a new breed of talent with expertise in software development, cybersecurity, and data management.

Implementing software-defined vehicles

Shifting to software-defined vehicles will be a complex process that requires careful planning across multiple industry stakeholders. Automakers will need to reevaluate their approach to integrating software and hardware components. Hardware must be more flexible and modular in nature, compared to traditional vehicles that serve specific applications. The automotive industry has to integrate software development expertise and adopt new design and test methodologies to realize a more software-driven future.

Automotive suppliers will need to prioritize cybersecurity and data privacy to ensure SDVs are not vulnerable to cyberattacks. As SDVs collect and transmit data, clear guidelines are necessary on data ownership, privacy, and adherence to evolving regulations for autonomous vehicle software. Industry-wide standards for software platforms would enable faster innovation and wider adoption of SDVs. All these changes are necessary to facilitate SDV implementation and require thorough testing and validation processes.

History and future outlook of software-defined vehicles

The concept of software-defined vehicles is not entirely new, but it gained traction in the 2010s. Vehicles have gradually incorporated more software over the years, including features like engine management and basic infotainment systems. This growth laid the groundwork for the SDV concept.

Tesla often receives credit for popularizing the concept by focusing on OTA software updates and features, like smartphones, but all automakers recognize the importance of software in modern vehicles.  While Tesla might be a frontrunner, other manufacturers are actively developing their own SDV strategies to keep pace with evolving consumer demands for the latest features and functionality. The future of SDVs continues to unfold, with expectations of playing a significant role in the ongoing transformation of the automotive industry.

Current industry trends and technological advancements

The SDV landscape is ripe with innovation, and collaboration is key to unlocking these opportunities. OEMs are actively building their software development capabilities, either organically or through partnerships with tech giants like Amazon and Google. Automakers are also forging partnerships with chipmakers like NVIDIA and Qualcomm to leverage advanced processing power for more advanced features, like higher levels of ADAS. These partnerships reflect the growing importance of software in vehicle design and function.

The greater focus on software has facilitated more standardized hardware platforms across different vehicle models, streamlining the development process for software features and allowing automakers to focus their efforts on software innovation. SDVs are increasingly connected to the cloud, enabling features like real-time traffic updates and remote diagnostics. Artificial intelligence (AI) is also playing a growing role in SDVs, unlocking the ability to improve ADAS features, personalize in-car experiences, and even pave the way for SAE Levels 4 and 5 autonomous vehicles. These trends and advancements are shaping the future of the automotive industry.

Future developments and innovations

The future of software-defined vehicles is brimming with possibilities. The following are some exciting developments and innovations that SDVs are propelling:

  • Advanced personalization: Software-driven construction can cater to specific driver or passenger preferences. Biometric recognition could adjust seat settings, temperature, infotainment options, and even provide route recommendations based on who is in the vehicle.
  • Predictive maintenance: SDVs constantly monitor their own performance and predict potential issues before they arise. This enhancement could revolutionize car maintenance, with vehicles even recommending service appointments automatically.
  • Vehicle-to-Everything (V2X) communication: SDVs enable seamless communications with other vehicles, traffic lights, and even infrastructure. This ability could lead to smoother traffic flow, reduced accidents, and even optimized routes based on real-time data.
  • Cybersecurity advancements: As SDVs become more reliant on software, robust cybersecurity measures will be crucial to prevent hacking attempts. Software-defined vehicles could drive advancements in encryption, intrusion detection systems, and secure communication protocols.
  • Mobility-as-a-Service: SDVs could play a major role in the growth of MaaS, where car ownership becomes less prominent and on-demand access to various types of vehicles becomes the norm. Software features could personalize the MaaS experience, allowing users to seamlessly rent and utilize vehicles that adapt to their specific needs.

These developments provide just a glimpse into the future with SDVs. As software technology continues to evolve, more innovative features and functionalities will emerge — fundamentally changing the way users interact with and experience their vehicles.

Keysight's role in software-defined vehicle development

Keysight is the leader in the automotive testing and measurement industry. The company plays a crucial role in developing software-defined vehicles by providing the solutions and expertise necessary for testing and validating the complex software components that power these vehicles.

  • Test and validation: Keysight offers a wide range of test and validation solutions specifically designed for SDVs, including tools for simulating real-world driving scenarios, testing in-vehicle networks, and ensuring compliance with industry standards for automotive software.
  • Emulation: Keysight's solutions can emulate complex traffic scenes and various driving conditions, enabling customers to thoroughly test features like ADAS and autonomous driving functionalities in a safe and controlled environment.
  • Connectivity: Keysight provides solutions for testing OTA updates and V2X communications to ensure vehicles can communicate seamlessly and securely with external systems.
  • Security: Keysight offers cybersecurity tools and expertise to help automakers identify and address vulnerabilities in their vehicles' software. These solutions and services help safeguard against hacking attempts and other security threats.

Keysight acts as a strategic partner for SDV developers by providing the equipment to test and validate the functionality of the software at the heart of these next-generation vehicles. Keysight solutions help to ensure the safety, reliability, and performance of SDVs as they hit the road.

Discover related use cases

Access additional resources

Accelerate your SDV innovation

Leverage Keysight's deep domain knowledge and industry-leading design, emulation, and test solutions to accelerate the development of your SDV technology.

A 3D illustration of a software-defined vehicle sending out a signal

Software-Defined Vehicles – Frequently Asked Questions

Software-defined vehicles provide the opportunity for enhanced performance and efficiency, improved vehicle and road safety, evolving vehicle capabilities, a more personalized driving experience, and predictive maintenance. As vehicles become more software-driven, more capabilities can be realized over the lifetime of the vehicle rather than having to be finalized when it is produced.

The challenges of developing and implementing software-defined vehicles include the sheer software quantity and complexity, cybersecurity threats, data privacy concerns, shift to modular hardware and software and technical expertise gap in the workforce. Many of these challenges are being addressed currently and are not expected to hold back the advancement of SDVs.

Software-defined vehicles are transforming how the automotive industry approaches vehicle design, development, manufacturing, and support. Traditional vehicles offer limited functionality and features while SDVs remain constantly evolving and adaptable through ongoing software updates. This software-driven transformation is seen as a significant evolution in the automotive industry — paving the way for further technological advancements like autonomous vehicles.

Want help or have questions?