Keysight Delivers Significant Enhancements to 5G Network Emulation Solution Platform, Accelerating Development of 3GPP Rel-16/17 Device Designs

Enables chipset and device makers to launch advanced 5G features quickly and confidently

SANTA ROSA, Calif. March 4, 2022 

Keysight Technologies, Inc. (NYSE: KEYS), a leading technology company that delivers advanced design and validation solutions to help accelerate innovation to connect and secure the world, has delivered a range of enhancements to the company's 5G Network Emulation Solution that support the latest 3GPP Rel-15/16/17 features, and enable leading chipset and device makers to quickly and confidently develop designs with advanced 5G capabilities for consumer, industry and government applications.

Over the past year, the new updates have enabled leading 5G chipset makers to develop and verify the performance of advanced 5G chipsets based on 3GPP release 16 (Rel-16), supporting new features and capabilities. Expected to be introduced to market in 2022, these chipsets have already been tested and verified using Keysight's enhanced 5G network emulation solution, based on the company's UXM 5G Wireless Test Platform. Keysight has used the enhanced network emulation platform to realize several industry-first 5G achievements in collaboration with these leading chipset makers. Industry milestone achievements include the first 10 Gbps downlink (DL) IP data throughput demonstration in June 2021 and the first 3.5 Gbps UL IP data throughput demonstration in January 2022.

"We're pleased to enable a global 5G ecosystem to capture early market revenue opportunities by delivering industry-first enhancements to Keysight's Network Emulation portfolio, providing double the capabilities of the original solution launched in 2017," said Cao Peng, vice president and general manager of Keysight's wireless test group. "We're witnessing the first commercial deployments of 3GPP Rel-16 this spring and expect to see early implementations of Rel-17 towards the end of 2022. Keysight's 5G test solutions have, and will continue to, provide a future-proof test platform for chipset makers, device manufacturers, mobile network operators, test labs, system integrators and operational technology (OT) vendors to rapidly develop and verify 5G devices and networks."

Key enhancements to Keysight's network emulation platform include:

  • Extended frequency range (FR) coverage, providing support for the sub-8GHz FR1 extension into the new licensed and unlicensed bands (NR-U), high intermediate frequency (IF) support for FR2 testing, and the new 47 GHz mmWave FR2 band n262.
  • Flexible use of new wider bandwidth RF resources to provide superior EN-DC and NR-DC band combination coverage, providing one-box support for 8 component carriers (CC) in 8 FDD/TDD bands with 4x4/2x2 MIMO.
  • Increased processing power to support more carrier aggregation (CA) with >10CC, and higher data throughput rates beyond 10 Gbps end-to-end IP for data-intensive use cases including 8K video streaming.
  • Enhanced uplink (UL) capabilities to support UL antenna switching, multi-Angle of Arrival (AoA) testing, and more CCs for UL CA to enable HD video and image sharing and livestream use cases.
  • New Rel-16 Ultra Reliability & Low Latency Communication (URLLC) features, enabling devices serving the Industrial IoT (IIoT), Private Networks, Time-Sensitive Networking (TSN) and extended reality (XR) markets.
  • Comprehensive multi-SIM support, including Dual-SIM Dual-Active (DSDA) for 5G/4G network combinations.

Keysight's 5G network emulation solution leverages the company's UXM 5G Wireless Test Platform, an integrated and compact signalling test platform with multiformat stack support, rich processing power and abundant radio frequency (RF) resources, to emulate a 5G new radio (NR) network. The UXM 5G platform supports RF characterization, protocol compliance and functional key performance analytics across both sub-6GHz and mmWave spectrum. Solution updates are available in a range of new platform configurations and price points to support RF protocol, functional and performance use cases across the device workflow. 

About Keysight Technologies   

Keysight delivers advanced design and validation solutions that help accelerate innovation to connect and secure the world. Keysight's dedication to speed and precision extends to software-driven insights and analytics that bring tomorrow's technology products to market faster across the development lifecycle, in design simulation, prototype validation, automated software testing, manufacturing analysis, and network performance optimization and visibility in enterprise, service provider and cloud environments. Our customers span the worldwide communications and industrial ecosystems, aerospace and defense, automotive, energy, semiconductor and general electronics markets. Keysight generated revenues of $4.9B in fiscal year 2021. For more information about Keysight Technologies (NYSE: KEYS), visit us at www.keysight.com.

# # #

Additional information about Keysight Technologies is available in the newsroom at https://www.keysight.com/go/news and on Facebook, LinkedIn, Twitter, and YouTube.

Keysight Contact:

Geri Lynne LaCombe, Americas/Europe
+1 303 662–4748
geri_lacombe@keysight.com

Fusako Dohi, Asia
+81 42 660–2162
fusako_dohi@keysight.com

Mexico