Highlights

Simplify Test Setup and Configuration

The Keysight WaveJudge offers a powerful graphical user interface that can be used on a standalone basis. Its strong visual emphasis on troubleshooting and configuration makes it a great tool for testing. The user-friendly software control package greatly simplifies test setup and provides quick graphic confirmation of the test configuration. Thanks to its powerful import and export features, its visual analysis tools can expand to troubleshoot in cross-platform environments.

KeysightCare Logo

Troubleshoot Challenging NTN Issues

Non-terrestrial Networks (NTN) bring challenges like path loss, propagation delay, and time drift, making troubleshooting network issues harder. Rapidly capture IQ from different stages of the NTN chain and analyze all layers from PHY / RF to L1-L3 using Keysight WaveJudge Wireless Analyzers. This solution decodes LTE, 5G, and Wi-Fi® signals, offering real-time visibility into everything from protocol and physical layer interactions to root cause issues. The solution helps you troubleshoot faster and boost network quality.

WJ001000A Powerful Graphic Interface

Powerful Graphical User Interface

The WaveJudge offers a powerful graphical user interface (GUI) that simplifies the test setup and configuration. Using the GUI, you can:

  • Identify and analyze complex antenna schemes including MIMO and beamforming.
  • Compare expected versus received frame structure and identify allocation issues.
  • Synchronize and reference signal errors.
  • Visually inspect scheduler performance.
  • Capture the attach process beginning with UL power.
  • Trace the bytes as they move through the MAC, RLC, and PDCP layers.

Cross-Platform Import and Export Features

WaveJudge can troubleshoot different environments and various system interfaces thanks to its powerful import and export features. These are the IQ captures it supports:

  • Keysight E7515B UXM 5G
  • Keysight VSA (89600)
  • Keysight ORAN Studio
  • Keysight Propsim Channel Emulator
  • Keysight UeSIM UE Emulator
  • Keysight WaveJudge
Cross-Platform Import and Export Features

SJ001A WaveJudge Wireless Analyzer Toolset

The WaveJudge Wireless Analyzer Toolset combines powerful over-the-air communications analysis, real-time protocol decoding, and PHY analysis. It is an essential tool for troubleshooting 5G network performance problems between devices and base stations in development and deployment.

Characterize 5G NR RedCap Devices

RedCap stands for Reduced Capability 5G NR devices. The 3GPP approved this new device type in Release 17 to make it easier for 5G to work with IoT devices. The reduced 5G NR capability means lower costs during development and manufacturing. Typically, IoT uses low-cost devices in applications such as wearables, industrial sensors, smart homes and cities, and security and surveillance. Learn more about how our wireless network emulation solutions help to reduce cost while performing functional and RF tests on RedCap devices.

Want help or have questions?

Italy