Keysight Launches Wireless Test Platform for 5G RedCap and Cellular IoT Industry Progression

  • Provides chipset, device, and module maker ecosystem with a network emulation platform designed specifically for all cellular internet of things technologies, including the 5G RedCap specification
  • Supports the entire cellular internet of things development workflow, from early design and development to deployment

SANTA ROSA, Calif. February 22, 2023 

Keysight Technologies, Inc. (NYSE: KEYS), a leading technology company that delivers advanced design and validation solutions to help accelerate innovation to connect and secure the world, announced its new E7515R solution based on its 5G Network Emulation Solutions platform, a streamlined network emulator specifically designed for protocol, radio frequency (RF), and functional testing of all cellular internet of things (CIoT) technologies, including RedCap. The E7515R expands Keysight's 5G Network Emulation Solutions portfolio, the industry's most robust, which is used in mobile device validation across the workflow, from early design to acceptance and deployment. 

The 5G RedCap specification introduces support for wireless devices with reduced 5G capabilities. These devices are less complex, and consume less power, allowing them to address new CIoT use cases such as industrial sensors and wearables such as smartwatches. Like other cellular devices, RedCap devices require time-consuming and expensive certification from accredited labs before they can be released to the market. By performing lab validation ahead of time to identify and correct design issues, device and module manufacturers can shorten the certification process for RedCap and other CIoT devices.

The Keysight E7515R addresses this need as a network emulation test platform designed specifically for 5G RedCap and supporting all CIoT technologies. The solution features streamlined capabilities for RedCap without the additional features needed to test a full-spec 5G device.

The E7515R solution delivers the following benefits:

  • Specifically built for RedCap and CIoT: The E7515R supports 5G Release 17 RedCap along with legacy CIoT technologies, including Narrowband IoT (NB-IoT), LTE Category M, and LTE Cat-1bis.
  • Integrated Platform: The E7515R is a complete solution offering RF, protocol, functional, and performance testing in a compact footprint.
  • Built on Keysight's Proven Technology: The E7515R is built on the same architecture as the market-leading 5G Network Emulation Solutions platform. The E7515R uses the same proven software solutions employed by the 5G Network Emulation Solutions platform, providing workflow consistency and reduced learning curves.
  • End-to-End Solution: The E7515R supports the entire RedCap and CIoT device development workflow, from early design and development through acceptance and certification testing, and deployment.

The release of the E7515R solution builds on Keysight's ongoing achievements supporting RedCap device development, including establishing a data call using the 5G RedCap specification. Through this demonstration, Keysight's 5G Network Emulation Solutions validated RedCap connectivity on a 5G chipset.

Mosaab Abughalib, General Manager of Keysight's Wireless Device Development R&D Group, said: “With the introduction of the E7515R solution, Keysight is providing chipset, module, and device makers with a proven test solution that enables the development workflow of the next generation 5G New Radio (NR) RedCap devices. The E7515R solution is optimized for the development of devices that do not require full 5G NR capability, which allows our customers to maximize their return on investment.”

The E7515R is shipping now and Keysight will demonstrate the solution's 5G RedCap network emulation capabilities at Mobile World Congress 2023, Hall 5 Stand 5E12.

Resources

About Keysight Technologies   

Keysight delivers advanced design and validation solutions that help accelerate innovation to connect and secure the world. Keysight's dedication to speed and precision extends to software-driven insights and analytics that bring tomorrow's technology products to market faster across the development lifecycle, in design simulation, prototype validation, automated software testing, manufacturing analysis, and network performance optimization and visibility in enterprise, service provider and cloud environments. Our customers span the worldwide communications and industrial ecosystems, aerospace and defense, automotive, energy, semiconductor and general electronics markets. Keysight generated revenues of $5.4B in fiscal year 2022. For more information about Keysight Technologies (NYSE: KEYS), visit us at www.keysight.com. 

# # #

Additional information about Keysight Technologies is available in the newsroom at https://www.keysight.com/go/news and on Facebook, LinkedIn, Twitter, and YouTube.

Keysight Contact:

Geri Lynne LaCombe, Americas/Europe
+1 303 662–4748
[email protected]

Fusako Dohi, Asia
+81 42 660–2162
[email protected]

The Keysight E7515R solution is a streamlined network emulator designed to provide protocol, radio frequency, and functional testing of all cellular internet of things technologies, including RedCap.