Keysight First to Submit Protocol Conformance Test Case for 3GPP Release 17 Non-Terrestrial Networks Standards

  • Verified test case submission includes protocol conformance for narrowband internet of things hosted over non-terrestrial networks
  • Test case will enable device and module makers to begin verifying standards compliance of designs supporting advanced NTN features

SANTA ROSA, Calif. July 21, 2023 

Keysight Technologies, Inc. (NYSE: KEYS) has submitted the first protocol conformance test case for the 3rd Generation Partnership Project's (3GPP) Release 17 (Rel-17) standards for non-terrestrial networks (NTN) using narrowband internet of things (NB-IoT) technology. The submission was verified using the Keysight Protocol Conformance Toolset

Based on satellite-to-ground communication, NTNs bring secure, reliable, and high bandwidth connectivity to remote areas that do not have terrestrial network coverage. Widespread NTN deployments can improve economic conditions in remote areas with industries such as agriculture, energy, health, and transportation using low-cost and low-powered NB-IoT devices for applications including remote sensing, asset tracking, and surveillance.

Keysight's Protocol Conformance Toolset provides a comprehensive suite of test cases prioritized by the Global Certification Forum (GCF) and the PTCRB that is used to certify the standards compliance of new mobile devices. Once the test case is approved by the 3GPP, network equipment, chipset, and device makers will be able to speed market introductions of devices and modules supporting advanced NTN features.

Muthu Kumaran, General Manager, Keysight, said: "This 3GPP Release 17 NB-IoT NTN test case submission underscores Keysight's leadership in the NTN device ecosystem and our commitment to giving the industry the tools it needs to rapidly adopt new 3GPP specifications and roll out new devices."

About Keysight Technologies   

At Keysight (NYSE: KEYS), we inspire and empower innovators to bring world-changing technologies to life. As an S&P 500 company, we're delivering market-leading design, emulation, and test solutions to help engineers develop and deploy faster, with less risk, throughout the entire product lifecycle. We're a global innovation partner enabling customers in communications, industrial automation, aerospace and defense, automotive, semiconductor, and general electronics markets to accelerate innovation to connect and secure the world. Learn more at Keysight Newsroom and www.keysight.com

Keysight Contact:

Paul Erwin, Americas/Europe
+1 248 430–9075
[email protected]

Fusako Dohi, Asia 
+81 42 660–2162
[email protected]