Source / Measure Units

An image of an integrated circuit (IC) being tested using an SMU in the semiconductor industry

Match the right precision, speed, resolution, and density

Testing complex systems like low-power integrated circuits or automotive systems at a high degree of reliability and qualification is a challenging task. Learn how a source / measure unit (SMU) can help you overcome key obstacles in application-specific tests, including low-power integrated circuits tests, low-current LED tests, vertical-cavity surface-emitting laser (VCSEL) sensor / module tests, narrow pulsed light-current-voltage (LIV) tests, DC bias sourcing tests for optical receivers and modulators, data center applications, and more.

Learn the essentials of using an SMU

Learn the basics of source meters

SMU Basics

Learn the basics of a source / measure unit (or source meter), an instrument that measures direct current (DC) or voltage while simultaneously sourcing / supplying or sinking / receiving them.

Learn the different types and form factors of SMUs

SMU Types Explained

Explore the various form factors of SMUs and how to select the correct type to optimize performance for a given application. Evaluate the pros and cons of the SMU categories and their operation modes.

Learn the different operation modes available in an SMU

SMU Operation Modes Explained

Dive into the multiple modes of operation typically offered in a source meter. Understand when to use the normal, power supply, high capacitance, or laser diode mode.

Learn about the characteristics of electrical materials

Sheet Resistivity Explained

Learn in-depth about sheet resistivity, a fundamental characteristic of electrical materials. Understand how to use a source / measure unit to perform sheet resistance measurements in semiconductor device testing.

Learn about an SMUs digitizer mode

SMU Digitizer Mode Explained

Understand the function of an SMU digitizer mode and its practical applications. Learn to excel at the triggering control system of an SMU and capture transient events more efficiently than using the timer trigger function.

Featured courses

Discover SMU applications

Low power ic test using a high channel density source measure unit
Source measure unit for VCSEL LIV test
Source measure unit for optical device test
Source measure unit for quantum computing
Source measure unit for LED test
High Density Precision SMU solution with IV Curve Measurement Software

Focus More on Characterization and Less on Synchronization

Learn how to use an SMU to overcome five key challenges in testing low-power integrated circuits and how it enables you to focus more of your time on testing rather than implementation details.

SMUs: Go deeper

Learn how an SMU can help overcome your test and validation challenges with application notes from Keysight engineers

Related use cases

learn more

Dive into more insights and questions on SMUs

Watch this on-demand webinar, which will address your most pressing questions regarding high-density precision source / measure unit (SMU) testing.
learn more

SMU Solutions

Find the source measure unit that's right for you
source measure unit

Claim Exclusive Reward When You Purchase an SMU

Get an exclusive free gift to complement your purchase of an SMU, enabling you to test with confidence. 
contact us logo

Get in touch with one of our experts

Need help finding the right solution for you?