Keysight Technologies First to Receive FCC Spectrum Horizons License for Developing 6G Technology in Sub-Terahertz

Accelerates development of technology supporting data-intensive high-bandwidth applications and sensing

SANTA ROSA, Calif. March 8, 2022 

Keysight Technologies, Inc. (NYSE: KEYS), a leading technology company that delivers advanced design and validation solutions to help accelerate innovation to connect and secure the world, has been granted the first Federal Communications Commission (FCC) Spectrum Horizons Experimental license for developing 6G technology in sub-Terahertz (THz) frequency bands, between 95 gigahertz (GHz) and 3 THz. 

The FCC license enables Keysight to develop cutting-edge technology used by researchers in academia and the industry to accelerate innovations that support data-intensive high-bandwidth applications, imaging and sensing. Keysight is also the first company to be granted FCC licenses above 246 GHz and 275.5 GHz. Access to large swaths of contiguous spectrum in sub-THz frequencies allows 6G innovators to realize high data throughput speeds of 100 giga bits per second (Gbps) up to 1 terabit per second (Tbps), as well as ultra-low latencies across short distances.

"Innovations in sub-THz spectrum will support use-cases such as immersive telepresence, digital twins and extended reality, which is all real-and-virtual combined environments and human-machine interactions generated by computer technology and wearables," said Roger Nichols, Keysight's 5G & 6G program director. "Using the FCC Spectrum Horizons license enables Keysight to strengthen our commitment to 6G technology, which will allow innovators to pioneer across the novel terrain of future-generation communications systems."

Keysight applied for the FCC licenses to promote 6G technology development while also ensuring no harmful interference to existing authorized users. The multiple FCC license grants follow Keysight's active participation in driving U.S. spectrum policy in consortia such as the mmWave Coalition, in which Keysight is a founding member. The mmWave Coalition is a group of innovative companies united in removing regulatory barriers to technologies and using frequencies ranging from 95 GHz to 450 GHz.

"The use of sub-THz spectrum to power the next generation of wireless technology is one key enabler to merging the physical and digital worlds, which will result in creative ways for people to interact with their surroundings," said Kailash Narayanan, president of Keysight's Communications Solutions Group. "Keysight takes an active role in several government-sponsored 6G initiatives around the globe. These are critical in generating momentum for technology that will accelerate digitalization and drive innovation for consumers, government and businesses."

About Keysight Technologies   

Keysight delivers advanced design and validation solutions that help accelerate innovation to connect and secure the world. Keysight's dedication to speed and precision extends to software-driven insights and analytics that bring tomorrow's technology products to market faster across the development lifecycle, in design simulation, prototype validation, automated software testing, manufacturing analysis, and network performance optimization and visibility in enterprise, service provider and cloud environments. Our customers span the worldwide communications and industrial ecosystems, aerospace and defense, automotive, energy, semiconductor and general electronics markets. Keysight generated revenues of $4.9B in fiscal year 2021. For more information about Keysight Technologies (NYSE: KEYS), visit us at www.keysight.com.

# # #

Additional information about Keysight Technologies is available in the newsroom at https://www.keysight.com/go/news and on Facebook, LinkedIn, Twitter, and YouTube.

Keysight Contact:

Geri Lynne LaCombe, Americas/Europe
+1 303 662–4748
[email protected]

Fusako Dohi, Asia
+81 42 660–2162
[email protected]