Keysight to Spotlight Solutions that Accelerate High-Speed Digital Innovations at DesignCon 2023

January 17, 2023 

 

What: Emerging technologies are driving high-speed digital standards to evolve rapidly, with each generational change introducing new test challenges. At DesignCon 2023, Keysight will demonstrate how it enables innovators to push the boundaries of engineering by quickly solving design, emulation, and test challenges to create the best high-speed digital experiences.

When: January 31 - February 2, 2023

Where: Keysight Booth Number 1039, Santa Clara Convention Center 

 

Join Keysight at the following sessions: Keysight Education Forum (KEF), technical presentations/papers, panel discussions, Chiphead Theater, and boot camps.

As a corporate exhibitor at DesignCon 2023, Keysight will showcase:

PathWave Advanced Design System 

  • Memory / SerDes Simulation: PathWave Advanced Design System (ADS) 2023 offers a cohesive design workflow for early design investigations and final product system verification, including three new innovations to speed development cycles and give the highest confidence in design sign-off.

High-Speed Computing Interfaces

  • PCI Express® 5.0 Protocol: New PCIe® 5.0 protocol test tools that offer emulation and packet decode up to 32GT/s in x4, x8, and x16 lane widths. CEM form factor simplifies connection to the device under test and offers superior signal integrity with real-time equalization and amplification to effectively remove the effects of the test tools from the link and provide extremely fast calibration of the test system to the device.

Pathway to 1.6T

  • 224 Gbps Rx Test: 1.6T receiver test solution characterizing 224 Gbps interfaces offering customers high bandwidth and signal integrity.
  • 212 Gbps Tx Validation: Automated test system for 224G physical layer (PHY) validation, spotlighting signal-to-noise and distortion ratio (SNDR), and jitter measurements.
  • 800 GE FEC and BER: A test solution measuring passive and active copper cable interconnect for 800GE devices and components and consisting of the G800GE-02 FEC error correction and Bit Error Ratio (BER) performance analyzer.

Consumer Electronics

  • USB 80 Gbps and DP 2.1: Showcasing Keysight’s portfolio of USB4 Version 2.0 solutions using the D9050USBC TX and RL application, N5991U42A RX application, PathWave ADS simulation solutions, UXR Series oscilloscope, and M8040A Series BERT.

Signal Integrity Analysis

  • Multi-Domain Characterization: A digital interconnect reference solution that enables multiport s-parameter calibration, measurement and analysis for high-speed digital interconnect using a modular PXI chassis.

DDR5 Memory Validation

  • DDR5 Simulation & Test: Spotlighting new measurement science performing DDR5 compliance on a simulated waveform for fast repeatable test and a data repository for quick result analysis and decision making.

Media Activities

Contact Geri LaCombe to schedule media briefings and solution demonstrations.

PCI-SIG®, PCIe® and the PCI Express® are US registered trademarks and/or service marks of PCI-SIG.

About Keysight Technologies   

Keysight delivers advanced design and validation solutions that help accelerate innovation to connect and secure the world. Keysight's dedication to speed and precision extends to software-driven insights and analytics that bring tomorrow's technology products to market faster across the development lifecycle, in design simulation, prototype validation, automated software testing, manufacturing analysis, and network performance optimization and visibility in enterprise, service provider and cloud environments. Our customers span the worldwide communications and industrial ecosystems, aerospace and defense, automotive, energy, semiconductor and general electronics markets. Keysight generated revenues of $5.4B in fiscal year 2022. For more information about Keysight Technologies (NYSE: KEYS), visit us at www.keysight.com. 

# # #

Additional information about Keysight Technologies is available in the newsroom at https://www.keysight.com/go/news and on Facebook, LinkedIn, Twitter, and YouTube.

Keysight Contact:

Geri Lynne LaCombe, Americas/Europe
+1 303 662–4748
[email protected]

Fusako Dohi, Asia
+81 42 660–2162
[email protected]