Keysight Technologies, Jiyun Technologies Collaborate to Deliver a Tailored, Compact Battery Test System

High-efficiency battery test system accelerates the launch of new electric vehicles

SANTA ROSA, Calif., September 21, 2022 

Keysight Technologies, Inc. (NYSE: KEYS), a leading technology company that delivers advanced design and validation solutions to help accelerate innovation to connect and secure the world, announced a collaboration with Jiyun Technologies to develop and deliver a tailored, compact battery test system for electric vehicles (EVs). 

Range limitations and safety concerns remain consumer obstacles for purchasing electric vehicles. To address these concerns and facilitate the rapid launch of new electric vehicles, solid testing and performance verification of battery systems is paramount. Keysight and Jiyun Technologies have joined forces to address these concerns.

Keysight delivered the tailored battery test system to Jiyun Technologies, which includes the company's regenerative power supplies (RPS7900 Series), Data Acquisition System (DAQ973A), Controller Area Network Interface (CAN) Bus communication interfaces and other hardware products. The dedicated test software leveraged in the battery test system was adopted from Keysight's PathWave software portfolio, and the custom system can reach a maximum output voltage of 1000V, a current level of up to 540A and a maximum power level of 180kW.

"New electric vehicles are developing rapidly and batteries, as the heart of electric vehicles, need to be taken seriously," said Xue Xianglei, R&D director at Jiyun Technology. "Jiyun is grateful to Keysight for providing a high-efficiency battery test system, which will help accelerate the launch of new products."

Keysight battery test system at Jiyun 

Keysight battery test system software used by Jiyun 

Keysight optimized the battery test system to be compact while meeting the needs of the tailored battery pack testing. In addition to collecting basic information such as battery voltage, current and thermal data, the battery management system (BMS) is also integrated into the communication structure to efficiently gather data and provide access to all parameters through a single software instance. 

Keysight also delivered a solution based on regenerative power components to achieve 90% power efficiency that reduced operational costs while minimizing heat dissipation, as well as reducing the associated costs of required cooling systems.

"The testing needs for electrical vehicles will pose a challenge for the foreseeable future and depending on specific customer needs, solution offerings need to be adaptable," stated Jian-Rui Ma, China business manager for the Automotive and Energy business unit at Keysight Technologies. "We appreciate the opportunity and challenge to work with Jiyun Technologies to develop a solution that is tailored to their specific requirements."

About Keysight Technologies   

Keysight delivers advanced design and validation solutions that help accelerate innovation to connect and secure the world. Keysight's dedication to speed and precision extends to software-driven insights and analytics that bring tomorrow's technology products to market faster across the development lifecycle, in design simulation, prototype validation, automated software testing, manufacturing analysis, and network performance optimization and visibility in enterprise, service provider and cloud environments. Our customers span the worldwide communications and industrial ecosystems, aerospace and defense, automotive, energy, semiconductor and general electronics markets. Keysight generated revenues of $4.9B in fiscal year 2021. For more information about Keysight Technologies (NYSE: KEYS), visit us at www.keysight.com.

# # #

Additional information about Keysight Technologies is available in the newsroom at https://www.keysight.com/go/news and on Facebook, LinkedIn, Twitter, and YouTube.

Keysight Contact:

Geri Lynne LaCombe, Americas/Europe
+1 303 662–4748
[email protected]

Fusako Dohi, Asia
+81 42 660–2162
[email protected]