military woman working on a computer network

What is Network Modeling?

Computer and communication networks play indispensable roles in both commercial and military domains, permeating into our personal lives at an accelerating pace. These networks are tasked with delivering reliable service across a myriad of operational conditions. Understanding how the network performs under varying circumstances is crucial. Reliability requirements differ depending on the type of application; for instance, email services have different reliability expectations compared to video streaming or telephony, which demand stringent quality of service (QoS). Moreover, the requirements for a soldier requesting fire support contrast with those of a user downloading a song or video clip. Unplanned stressors like denial-of-service attacks or sudden surges in user activity can severely impact network performance. While deploying the physical network for testing under different conditions is one approach, it is costly, resource-intensive, and may not be feasible for large-scale deployments or certain types of cyberattacks.

The Role of Network Modeling in Problem Solving and Optimization

Network modeling presents an efficient, cost-effective solution to assess network behavior under diverse operating conditions through simulation. Results derived from these simulations can be analyzed to evaluate network performance, pinpoint potential issues, understand their root causes, and address them proactively before deployment. Conducting simulations in a laboratory environment is faster and less expensive compared to live tests, enabling the exploration of different alternatives before network deployment or modifications.

Network modeling empowers planners, commanders, and operators to address many network-related inquiries. For example, a cellular carrier might utilize network modeling to determine the optimal network configuration capable of provisioning a specific number of simultaneous video streams while maintaining dropped call rates within acceptable thresholds. Similarly, a military commander could leverage network modeling to ensure critical communication messages, such as 'call for fire' requests, are routed swiftly even under compromised operating conditions. Additionally, an IT manager might employ network modeling to evaluate the capacity of their Wi-Fi network to accommodate additional video streams after migrating to a new standard like 802.11ax.

Furthermore, network modeling aids in assessing network resilience to cyberthreats, evaluating vulnerability levels, and the effectiveness of countermeasures without subjecting the physical network to actual cyberattacks. This minimizes the risk of exposing live assets to potential threats and leakage of attack vectors.

hooded person hacking into a network system

5G Network Modeling: Enhancing Performance Prediction and Optimization

As communication technologies evolve, such as 5G, network modeling becomes even more critical. With the introduction of 5G networks, characterized by high data rates, ultra-low latency, and massive connectivity, accurate modeling becomes essential for predicting network behavior and optimizing performance. 5G network modeling enables researchers, engineers, and network architects to simulate and analyze the impact of various factors like network architecture, radio wave propagation, and deployment scenarios on overall network performance. By using advanced simulation tools like Keysight Exata, professionals can design, analyze, and optimize 5G communication networks, bridging the gap between theoretical design and real-world deployment.

Network modeling offers a practical approach to understanding and optimizing network performance across diverse operating conditions. Whether it is for commercial applications, military operations, or cybersecurity, network modeling provides a low-cost, low-risk means of predicting behavior, identifying potential issues, and implementing effective solutions before deployment.

Introducing Keysight EXata: Advanced Network Modeling and Simulation Software

EXata stands as a pinnacle in network modeling and simulation software, offering a suite of tools that empower researchers, engineers, and network architects alike. Whether your focus lies in wireless, wired, or hybrid networks, EXata provides a comprehensive platform for designing, analyzing, and optimizing communication networks. By facilitating rigorous testing and validation of network protocols, applications, and services, EXata seamlessly bridges the gap between theoretical network design and real-world deployment. For network professionals worldwide, EXata emerges as an indispensable tool, ensuring robustness and reliability in network infrastructures.

Watch for the continuation of this series where we will delve deeper into the purpose and functionality of network modeling.

limit
3