Können wir Ihnen behilflich sein?
Keysight Technologies to Showcase Advanced High-Speed Digital Design Solutions at DesignCon 2021
What: High-speed digital standards are evolving, and technological generational changes introduce new test challenges for digital designs. At DesignCon 2021, Keysight's technical experts will highlight high-speed digital designs across all product development stages which enables customers to anticipate test challenges and optimize performance, as well as accelerate time-to-market of high-speed computing interfaces, data center connections and consumer electronics.
When: August 16 – 18, 2021
Where: Keysight Booth Number 807
San Jose McEnery Convention Center
Expo Information
Tuesday, August 17, 2021: 11 a.m. - 6 p.m. PDT
Wednesday, August 18, 2021: 11 a.m. - 6 p.m. PDT
Keysight will deliver the following demonstrations that help accelerate a customer's digital designs:
- PathWave Design
- PathWave Advanced Design System (ADS) and workflow wizards to reduce design iterations in next-generation memory system designs.
- High-Speed Computing Interfaces
- PCI Express (PCIe) transmitter (Tx) and receiver (Rx) test solutions (PCIe5 and PCI6 pathfinding) that examine signal integrity challenges, issues with connector crosstalk, receiver jitter sensitivity, overall channel insertion loss and attenuated signals.
- Input/output buffer information specific (IBIS) algorithmic modeling interface (AMI) models on an enhanced double data rate (DDR5) bit-by-bit channel simulator that provides signal access, automated control of the device under test (DUT) for fast repeatable test and a data repository for quick result analysis and rapid decision making.
- Data Center Connectivity
- An automated test system for 100 Gbps physical layer (PHY) validation (800G) which requires unique, precision measurements to validate new test methods and specifications before the standard is complete.
- A compliance test solution for 400GBASE devices and components to achieve increased bandwidth in data center networks and designed to integrate forward error correction (FEC) constraints into the physical design validation.
- Consumer Electronics
- USB4 and DisplayPort 2.0 compliant solutions over a lossy (using inexact approximations and partial data discarding to represent content), low cost, passive cable with Keysight's UXR-Series oscilloscope.
- Signal Integrity
- Offering insight into associated signal integrity challenges such as reflections, eye diagram closure, crosstalk, and bit errors at the receiver for up to 800G physical layer interconnect components.
- Intelligent Software Test Automation
- How to enable companies to view their technology through the eyes of their users to identify and address interface errors and performance issues before they go into production.
In Executive Ballroom Room 210E, Keysight's test and measurement experts will offer complimentary Keysight Education Forum (KEF) sessions:
Tuesday, August 17th Sessions
- Advanced Testing Challenges at 32GBaud PAM4 with PCIe 6.0
- Next Gen Development in Type-C Ecosystem
- Physical Layer Validation Challenges of Characterizing 100 Gbps/lane Designs
- Solving Forward Error Correction Problems
Wednesday, August 18th Sessions
- Guide to Recalibrate Signal Integrity Intuition for Memory Interfaces
- Ramping up on the Latest Skills for Power Integrity Design/Debug
- Next-Generation Memory Solutions
- Explore Why Testing Disaggregated 5G Elements in Isolations is Required to Ensure Proper O-RAN Fronthaul Conformance
In addition, on Tuesday, August 17th, visit the Chiphead Theatre from 2:15 to 3:00 p.m. for Keysight's Modernization of Test and Measurement technical session.
Additional information about the event is available at: https://www.keysight.com/us/en/events/america/tradeshows/designcon.html
Media Activities
Contact Geri LaCombe to schedule media briefings and solution demonstrations.
About Keysight Technologies
Keysight delivers advanced design and validation solutions that help accelerate innovation to connect and secure the world. Keysight's dedication to speed and precision extends to software-driven insights and analytics that bring tomorrow's technology products to market faster across the development lifecycle, in design simulation, prototype validation, automated software testing, manufacturing analysis, and network performance optimization and visibility in enterprise, service provider and cloud environments. Our customers span the worldwide communications and industrial ecosystems, aerospace and defense, automotive, energy, semiconductor and general electronics markets. Keysight generated revenues of $4.2B in fiscal year 2020. For more information about Keysight Technologies (NYSE: KEYS), visit us at www.keysight.com.
# # #
Additional information about Keysight Technologies is available in the newsroom at https://www.keysight.com/go/news and on Facebook, LinkedIn, Twitter, and YouTube.
Need to contact Media Relations at Keysight?